Part Number: ADS1261 We are designing a new industrial product with an expected production lifetime of 15 years. We are evaluating the ADS1261 as our primary ADC. Can TI confirm whether the ADS1261 is considered a long-term strategic product and whether…
Part Number: ADS1261
Hi Team,
We are using the ADS1261 in our design, where a single-ended input signal ranging from –2.5V to +2.5V is applied to the ADC input.
We have the following questions:
How should the AINCOM pin be connected in this…
Part Number: ADS1261 Hi!
I am currently using the TI ADS1261BIRHBR ADC in my design. I need to switch the reference source from AVDD to the internal 2.5V reference via a SPI command during operation.
Could you specify the required settling time before…
Part Number: ADS1261 Hi Team, I am using the ADS1261 ADC in a bipolar measurement application and need clarification on the achievable full-scale input range. System Conditions:
Analog supply:
AVDD = +2.5 V AVSS = −2.5 V
ADC configured for:
Bipolar…
Part Number: ADS1261-Q1 Other Parts Discussed in Thread: ADS1261 Communication issue with ADS1261:
Hello TI Support Team, I have designed a custom board based on ADS1261 intended to communicate with the Nucleo STM32F446RET6 board, which is not responding…
Part Number: ADS1261-Q1 Other Parts Discussed in Thread: ADS1261 Hello, I am seeking assistance with the ADS1261 regarding a specific inaccuracy during internal supply monitoring. While the ADC performs accurately for all external analog channels across…
Part Number: ADS1261 Other Parts Discussed in Thread: ADS124S06 Hi Team,
IUn our project we had a CS5524-ASZ from Cirrus Logic Inc., not it seems like about to reach EOL soon, so we plannig to use the ADS1261/ADS124S06 as a replacement for this part…
Part Number: ADS1261-Q1 Other Parts Discussed in Thread: ADS1261 Tool/software: Hi Team,
I am planning to use two ADS1261-Q1 for my application. I will using the provided SPI interface. There is Master microcontroller and 2 slave ADC connected on same…