Part Number: ADS1261 Tool/software: Hi,
I am trying to measure 4 load cell's data (4 differential outputs; unipolar supply) at 400 SPS with gain 64 for a force platform. I have designed a breakout board for ADS1261 to connect all the load cells to it…
Part Number: ADS1261 Tool/software: Dear Texas Instrument Team,
i build a temperature board (PCB) with your ADS1261 which kinda equals the EvalBoard ADS1261EVM.
When setting the reference (REF) to default (AVSS-AVDD) i need to divide the voltage for…
Part Number: ADS1261 Other Parts Discussed in Thread: ADS8598S , Tool/software: Hi Team, We are designing a data acquisition system that shall comply with the DO-160 military standard. In our system, we will be reading the data from the following sensors…
Part Number: ADS1261 Tool/software: Dear all, We are currently using in our design one ADS1261 chip with custom PCB and we are experiencing a strange issue with the reference voltage. Basically, we are acquiring a signal in "single ended mode", by connecting…
Part Number: ADS1261 Tool/software: Dear Texas Instruments support team,
i have designed a PCB with the ADS1261 and connections to my Raspberry Pi (see picture below).
The first step now is to talk to the ADC via SPI.
I wrote the following python…
Part Number: ADS1261 Tool/software: TI-ADS1261 ADC is always transmitting bytes with a value of zero over SPI bus back to master.
TI-ADS1261 Analog to Digital Converter is connected to Xilinx Zynq 7020 SOC (System On a Chip) through the Zynq SPI Bus…
Part Number: ADS1261
Tool/software:
Hello,
I am reading the TI application note "A Basic Guide to Bridge Measurements".
We have an application which requires 10V excitation. We have a bipolar +-2.5V source, and can get a bipolar +-5v source as…
Part Number: ADS1261
Tool/software:
Hi,
I am using an ADS1261 designing a force plate with four loadcells, my object is sampling the sensor at 1000hz, according to ads1261's datasheet tab8 and sbaa535a , when I use below parameters,
filter type…
Part Number: ADS1261 Tool/software: The original thread for this problem was closed as resolved but it is not resolved.
The original problem is that the TI-ADS1261 does not respond in the DOUT line to commands sent to it on the DIN from a Xilinx Zynq…
Part Number: ADS1261 Hello,
Is it possible to save on component count /complexity by synchronizing multiple ADS1261s so that AC Excitation is controlled by a single set of transistors and thus the excitation source can be shared across chips?
If so…