Part Number: ADS1262 Tool/software: Dear Team,
I've a question about the SPI timing of the ADS1262 device. The datasheet of the ADC says (Pg 10) that the delay time td(CSSC) from CS falling edge and first SCLK rising edge shall be 50 ns. But the sampling…
Part Number: ADS1262 Other Parts Discussed in Thread: CC2640R2F Hi TI team,
I am currently using the ADS1262 in a custom data-acquisition board, but I am observing inaccurate conversion results and unexpectedly large noise. I would appreciate your help…
Part Number: ADS1262 Tool/software: Hello,
I’m bringing up a three ADS1262 with an STM32H723 (SPI1 / HAL). I apply ~1.25 V between AINX–AINCOM, but the measured value is always 0 V (code = 0). This post is only about the voltage reading stuck at zero…
Part Number: ADS1262 Hi,
We are a subcontract manufacturer in the UK, we have ordered several batches of ADS1262IPWR and have a customer reporting issues on different batch code parts. We have received from TI store on our PO-168073, 250 pcs marked…
Part Number: ADS1262 Tool/software: Hi,
We have been using the ADS1262 on a datalogging product successfully for a few years. A recent batch of boards, which have this part fitted, have all exhibited a wildly different input impedance from those we…
Part Number: ADS1262 Hello,
I am designing a board using the ADS1262, and in my design, I would like to power the board via USB. I'm wondering if the input AVDD can reliably be powered by USB 5V, or if voltage variations could lead to unstable readings…
Part Number: ADS1262 Hello,
I need to design 4 ADCs in single PCB board. Any gap maintains (Placement) between two ADC's. I need to take care any extra points, please suggest to me.
Part Number: ADS1262 Tool/software: I am using this ADC to measure low voltage for a particular detector. In my design, the configuration is AVDD 2.5V, AVSS -2.5V, External Ref 1.25V, Sync 4, 32 Gain.
With help of Mr, Keith Nicholas, I could gain a…
Part Number: ADS1262 Tool/software: Hi TI community,
I'm using the ADS1262 for a precision measurement application. I've configured the ADC with the following settings:
CHOP mode enabled
SINC4 digital filter
Data rate: 10 SPS
…
Part Number: ADS1262
Tool/software:
Dears,
For ADS1262IPW, if it is single-ended input, all ten channels AIN0-AIN9 can be used, right? AINCOM is the reference ground terminal?
Many thanks!