Part Number: ADS1262 I'm using the ADS1262 with a custom pcb. I can read and write config registers perfectly fine but when I do a RDATA command I always get back 01111111 11111111 11111111 11111111 as the response no matter what.
Is there a common…
Part Number: ADS1262 Hello,
I am designing a board using the ADS1262, and in my design, I would like to power the board via USB. I'm wondering if the input AVDD can reliably be powered by USB 5V, or if voltage variations could lead to unstable readings…
Part Number: ADS1262 Hi,
I am working on ADS1262 ADC interfaced to FPGA (XC7A75TFGG676-2L). The control registers are programmed as:
POWER_REG= 0x01, INTERFACE_REG=0x00, MODE0_REG= 0x00, MODE1_REG=0x60, MODE2_REG=0x0B, MUX_REG=0x12. And ADC clock = 7.3728…
Part Number: ADS1262 Hi team,
Ads1262 has two ways to read ADC data , but one of that direct mode is not normal,(The ADC data maintains a single value)
below is Schneider's configuration, and ADC using Start pin to triggers conversion, could you help…
Part Number: ADS1262 Hello,
I need to design 4 ADCs in single PCB board. Any gap maintains (Placement) between two ADC's. I need to take care any extra points, please suggest to me.
Part Number: ADS1262 I am using the ADS1262 for high precision acquisition, the reference voltage is using the ADR4550, and the test signal source is using a 18650 lithium battery(4V ). Using the highest 2.5SPS sin4 mode, the code noise is about 21~22…
Part Number: ADS1262 Hi team,
My customer is using internal reference to provide reference voltage of another DAC device MAX5216, and bypassed by a 1uF capacitor, but find the output oscillating as below: Yellow waveform is REFOUT, Purple waveform is AVDD…
Part Number: ADS1262 Hi
I intend to use the ads1262 to mesure as PT100 Scanner. and becuase the temperature process is very slow I intend to use the ads at 2.5 sps . My question do I still need the anti aliasing filter ?
Part Number: ADS1262 Hello
The ADS1262 is reading successifully if the gain is 1 and the PGA is pypassed(MODE2 = 0x80) changing the MODE2 register to any other value will result in noisy unpredictable results . I want to use PGA = 32 .Please help. attached…
Part Number: ADS1262 Other Parts Discussed in Thread: ADS1263 , ADS1235 , ADS1261 Hi,
We are almost finished with the design of a product that uses the ADS1262 32bit ADC. Production is scheduled for May 2023.
Unfortunately these parts seem to be unavailable…