Part Number: ADS1278-SP Other Parts Discussed in Thread: ADS1278 Hi,
I have a copy of the IND grade SEE Test Report [Hirex, HRX/SEE/502, Issue:02, Jan 13 2016]
Is there an equivalent report for the SP grade device ?
Would it be possible to get a copy…
Part Number: ADS1278-SP Other Parts Discussed in Thread: ADS1278 , ADCPRO , ADS1278EVM-PDK Hi,
I installed the software for the evaluation board and unfortunately I receive the errors as shown below. I tried restarting the computer and that didn't help…
Part Number: ADS1278-SP Hello,
I would have news on the production and qualification for this MHFQ-MLS suffix (already approved by the DLA). DLA to audit the fabrication site has been completed?
Are there some any other evidence on QMLV qualification? …
Part Number: ADS1278-SP Other Parts Discussed in Thread: ADS1278 How can the ADS1278-SP be used in high speed (frame sync) TDM mode at 31.25 MHz if the DOUT1 timing is up to 31 ns?
The SP datasheet lists the SCLK and FSYNC to DOUT1 timing as taking up…
Part Number: ADS1278-SP Hi,
For a single ADS1278-SP system, is it required to assert SYNC* after power on?
The specification states:
"For consistent performance, re-assert SYNC* after device power-on when data first appear."
If there is no assertion…
Part Number: ADS1278-SP Hi,
tSPW, the SCLK positive or negative pulse width, is specified as 0.4 of tCLK, minimum.
The data sheet also says that the tCLK minimum is 37 ns, implying a maximum frequency of about 27 MHz.
And 0.4 x 37 ns = ~15 ns.
My question…
Part Number: ADS1278-SP Other Parts Discussed in Thread: ADS1278-HT , ADS1278 Hi sir,
Could you please help me to find out the automotive equivalent of ADS1278MHFQ having 84 pins
Part Number: ADS1278-SP Other Parts Discussed in Thread: ADS1278 Is fMOD rising edge aligned with SYNC in SPI mode? figure 69 appears to show that in SPI mode, there is a latency of tSCSU between clk and /SYNC risking edge. what is the latency between…
Part Number: ADS1278-SP Hello Team,
Just to confirm the dimension for the ADS1278MHFQ-MLS. when we convert the 13.81mm to mil will get 543.7 but in datasheet, it is mentioned as 350.77
Regards,
Renan
Part Number: ADS1278-SP Hello Team,
The datasheet of datasheet indicates that TID Radiation Lot Acceptance Test (RLAT) is TBD, Has this been completed? Can you share the report with us?
Regards,
Renan