Hi Gareth,
I'm not entirely sure what you mean by basic accuracy, but the gain error maxes out at 0.1%. There are still other error factors to take into consideration. You can learn more about various error sources in our TIPL series: https://www.ti…
Part Number: TPS25983 Hello team,
I am not able to change the cell value of NRETRY (D19) on TPS25983-CALC .
It says this sheet is being protected, and asks for a password. Could you give me password to unlock the protection?
Best Regards, Kei Kuwahara …
Part Number: TMP468 Hi all,
I was looking into the TMP468 and the Remote Optimization Tool Excel sheet available on ti.com
However, when attempting to run the the macro, I run into the following error below. Which library/function is missing from the…
Part Number: TPS40210 Hi Sir,
My cusotmer use TPS40210 at their PoE boost application.They use excel tool to calculate the setting of components. But there're some mismatch between excel tool and equations at datasheet. For example:
1. Inductor selection…
Hi Tommy,
In your calculation sheet, TJDCMAX is 267.6 C, which is more than the maximum allowable MOSFET junction temperature of 150 C. Hence, the derated SOA number is coming as negative.
Before using the design calculator, please refer to the datasheet…
Hi Daisuke-san,
Daisuke Maeda said: Was a heatsink used for the AM62x on the board used for measurements in the application note?
There was not one used. Instead a Thermal Flow System, TFS.
Daisuke Maeda said: What is the airflow (m/s) under temperature…
Hi Derek
Derek Roberson said: Is there not an excel tool for the BQ51013B? The [FAQ] Schematic Checklist for Wireless Power RX states that the FAQ applies to the BQ51013B and item #7 links to SLUC629
Bill J - I have updated the FAQ to point out BQ5105XB…
Part Number: TMS320F280038C-Q1 Hi,
there is a power estimation tool available for F28004x -> https://www.ti.com/tool/C2000-F28004X-POWER-EST-CALC
Is there something available or planned for F28003x ?
Thanks and best regards,
Gregor
Part Number: UCC5880-Q1 I'm trying to find the UCC5880-Q1 DESIGN CALCULATOR TOOL, you have made an excel for this series. I want to do a WCS( Worst Case Scenario) for a certain project and I would need an excel to complete it faster.