Part Number: ADS127L11 Other Parts Discussed in Thread: REF6041 , Hello,
Our customer consider to employ ADS127L11 with REF5050 instead of REF6041 on Typical Application circuit.
Q1.REF5050 "output voltage accuracy" is double number, but other than…
Part Number: ADS127L11 Other Parts Discussed in Thread: REF6041 , THP210 ,
Hello,
I would like to ask for support or a schematic review for the bipolar power supply of the ADS127L11+REF6041 and THP210.
I have a single-ended AC-coupled signal…
Part Number: ADS127L11 Other Parts Discussed in Thread: TIDA-010249 , ADS127L18 , ADS127L14 Tool/software: Hi Team,
We are searching for a ADC part with similar specification of ADS127L11, but we require dual differential channel. In ADS127L11, there…
Part Number: ADS127L11 Other Parts Discussed in Thread: REF6041 , THS4551 , , REF54 , REF70 , THP210
Tool/software:
Hi Team,
Customer choose REF4061 + ADS127L11 + THS4551 solution, under 1MSPS condition. He followed TI's recommendations exactly…
Part Number: ADS127L11 Other Parts Discussed in Thread: REF6141 Tool/software: Hello All! I have the following design where I am interfacing a signal (DC only) to the ADC via an opamp (with gain of 3) with the ADC being configured as a single ended one…
Part Number: ADS127L11 Tool/software: If a high level (3.3V) is input to the control signals (CLK, START, SDI, etc.) of the ADS127L11 when IOVDD = 3.3V and AVDD1,2 = 0V, is there a possibility that this could damage the device?
Part Number: ADS127L11 Other Parts Discussed in Thread: ADS127L21 , Tool/software: Hello, At the maximum, up to how many ADS127L11s can be connected in a daisy-chain configuration? How about ADS127L21? At the maximum, up to how many ADS127L21s can be…
Part Number: ADS127L11 Tool/software: Hi Ti team, We were observing a frequency shift on the data received from the ADS127L11 while giving a 10kHz sine from frequency generator we are able to observe ~65Hz shift (i.e . we are observing 10065 Hz after…
Part Number: ADS127L11 Hy,
in this forum is the following description :
"For debug purposes, after RESET, do not write to the registers and hold the START pin continuously high to see if the DRDY pin starts toggling (should be 400kHz). If not, then…
Part Number: ADS127L11 Other Parts Discussed in Thread: ADS127L21 If I need to sample at above 50 ksps the documentation indicates that I need to use the high speed mode that is good up to 400 ksps. However, if I need only (for example) 200 ksps, will…