Part Number: ADS127L11 Hi team,
How much is the digital input threshold voltage?
I can only see the data below in the datasheet.
What will the logic become when input 0.3*IOVDD~0.7*IOVDD?
Best regards,
Yuto
Part Number: ADS127L11 Hi team,
I got question about RESET / SCLK timing for td(RSSC).
As shown in Figure 6-3 in D/S, do we need to keep SCLK "Low" while td(RSSC) timing?
Or td(RSSC) is just a time that the communication has not started, thus…
Hello Lajos,
I checked your schematic and have a few comments.
1. Pinout and connections around ADS127L11 are correct and should work with no issues.
2. The reference circuit should work well as long as the reference pre-charge buffer is enabled in each…
Part Number: ADS127L11 Other Parts Discussed in Thread: TXU0101 Let's say I'm running the ADS127L11 with AVDD and IOVDD at +5V and AVSS at 0V and I want to provide CLK with the output from an external oscillator. What are the acceptable voltage…
Part Number: ADS127L11 Hi team,
I got a question about SPI Operation in D/S 9.1.1.
It says that:
1. Use an SCLK that is phase coherent to CLK; that is, ratios of 2:1, 1:1, 1:2, 1:4, and so on. 2. Minimize phase skew between SCLK and CLK (< 5 ns).
…
Part Number: ADS127L11 As I'm working through the ADS127L11EVM-PDK, I see the 127 has some different clock options. From the data sheet: Simply from a parts reduction/cost reduction/EMI standpoint, not having another oscillator on our board is appealing…
Part Number: ADS127L11 Other Parts Discussed in Thread: TINA-TI Hi all
My customer is evaluating the ADS127L11 and they have this question:
Is there a SPICE model for the ADC input available that they can use with LTSpice (their standard simulator) ? …
Part Number: ADS127L01 Other Parts Discussed in Thread: ADS127L11
Hi TINA TI experts,
Do you have any idea in how to connect ADS127L01 with STM32 via SPI in order to read data converted by ADC?
Is there any library of this ADC that can help me to do…
Part Number: ADS127L11 Hi all
My customer is evaluating the ADS127L11 and they find that for the AVDD1 supply a 3Ohm resistor is required (page 42 of the datasheet).
As 3Ohm is not a standard value:
They plan on using a 3.3Ohm 1% TK100 0603 thickfilm resistor…