Part Number: ADS127L21 Other Parts Discussed in Thread: ADS127L11 Tool/software: Hi, We are working on a project on which we are planning to use ADS127L21 as ADC input. But I am facing issue with the Linux driver of ADS127L21 . Could someone please provide…
Part Number: ADS127L21 Other Parts Discussed in Thread: ADS1271 , ADS8900B Tool/software: Hi,
for a new project we need a 24Bit ADC without internal digital Filter (or bypass option) currently we use ADS127L21, but as we understand the digital filter is…
Part Number: ADS127L21 Tool/software: Hello, in the datasheet of the ADS127L21 all interesting parameters are specified for AVSS=0V and AVDD1= 5V, that is to say, the analog part has unsymmetrical supply. I would like to use symmetrical supply with AVSS…
Part Number: ADS127L21 Tool/software: Hi Team
What is the SDO current drive capability? Is it 2mA
I need to connect the SDO to opto coupler and i need 6mA is it supported?
Thanks
Roey
Part Number: ADS127L21 Hi Team,
My customer has a question regarding ADS127L21 One-Shot Control Mode:
If One-Shot conversion is performed periodically, will there be latency through the filter for each conversion? Or is it just initial at the first measurement…
Hello Cheol,
The THS4561 will correctly adjust the output common mode to the level needed by the ADS127L21 since the VCM output of the ADS127L21 is connected to the VCOM input of the THS4561. If the ADS127L21 is powered from +/-2.5V supplies, then the…
Part Number: ADS127L21 Other Parts Discussed in Thread: INA851 , TPS7A39 , REF3425 , TPS709 , REF6025 Hi TI Team
Im planning to use the ADS127L21 in combination with an INA851. I use a +/-5 V supply for the INA851 and a +/-2.5 V supply for the ADC via a TPS7A39…
Part Number: ADS127L21 hello. This customer is using the ADS127L21 device.
Looking at the data sheet, there are a total of 4 Speed_mode. ①max-speed mode (Fclk=32.768Mhz) ①high-speed mode (Fclk=25.6Mhz) ①mid-speed mode (Fclk=12.8Mhz) ①low-speed mode (Fclk…
Part Number: ADS127L21 I am having trouble with the large input current of the IC.
AVDD1 = 5V AVDD2 = 5V AVSS = 0V REFP = 2.5V REFN = 0V IOVDD = 3.3V OSR 1024
AINP=4.5V Current 350uA AINN=0.5V Current 350uA
Since the input current is large as mentioned above…
Part Number: ADS127L21 Hi TI support team
I have a question regarding the M_CRC_ERR in the STATUS2 Register of the ADC. My config is: CONFIG1 = 0x03 CONFIG2 = 0x07 CONFIG3 = 0x67 FILTER1 = 0xE7 FILTER2 = 0x01 FILTER3 = 0x00 OFFSET2 = 0x00 OFFSET1 = 0x00 OFFSET0…