Other Parts Discussed in Thread: ADS1281 Hi,
In the ADS1281 datasheets appendix, there is a table referring to "session 1,2,3,4" and "scaling" 1/512, 1/8388608 and 134217728. Where do these numbers come from?
I need to know the FIR coefficients…
Other Parts Discussed in Thread: ADS1281 When I used ADS1281 and the different input arrival about 3V, the problem about amplitude limiting was appeared. The reading data is 0x5000000, and the MFLAG pin was high when the problem happened. The attachment…
Hi Matthew,
Welcome to the TI E2E Forums!
The ADS1281 (analog) supplies can be configured as unipolar (AVDD = +5V, AVSS = 0V), or bipolar (AVDD = +2.5V, AVSS = -2.5V).
The ADS1281 (analog) inputs are fully-differential and the input range is referenced…
Other Parts Discussed in Thread: ADS1281 Hi,
We're designing a system with multiple ADS1281 ADCs that must all be synchronized for a long period. The intent is to use the continuous sync mode. Could you discuss the workings of the continuous sync mode…
Hello,
I'm developing a high precision weighing scale based on electromagnetic force compensation. The main task is to measure a DC current with as much resolution and precision as possible. Here you can find the detailed documentation of the project…
Other Parts Discussed in Thread: ADS1281 Hi,
The phenomenon that described in the attached file occured.
Has someone ever seen the phenomenon?
and does someone know the reason of this phenomenon?
Thanks
GO
Bernd,
Just to add a little to what Luis has said, you may have had success running the clock faster than specified, but that doesn't mean it will work in every case from device to device and across temperature. You must adhere to the timing requirements…
Other Parts Discussed in Thread: ADS1281 , OPA1632 Hello,
I design an AD converter board with ADS1281 as prompted by the EVM . Can I put VCOM port of the OPA1632 also analog ground without REF5025 to use.
I want to use only bipolar operation. I think…
Other Parts Discussed in Thread: ADS1281 , ADCPRO Hallo
I have kit ADS1281EVM board with the MMB0 and want trigger conversion ADS1281EVM external logical signal, is it possible?
thanks for response Radek