Part Number: ADS1282 Other Parts Discussed in Thread: REF5025 , I am having trouble calculating the input voltage to the ADS1282. I am using a REF5025 as a voltage reference.
The ADS1282 is connected to a TI TIva TM4C1231D5PMT MCU.
The voltage on the input…
Part Number: ADS1282 Hi Team, seeking some clarification.
Currently trying to read a thermocouple using the ADS1282HPW, but have run into an issue where the adc is outputting in a way that makes it seem like the AINN2 is connected to ground rather than…
Part Number: ADS1282 Hi,
Good Day.
The customer would like to ask about ADS1282 and the possibility of underclocking the ADC.
He needs to check if it is possible to underclock ADS1282 ADC to achieve a final data rate of 100 SPS.
The ADC is working at 250…
Part Number: ADS1282-SP Wondering what CoTS equivalents there are for the ADS1282-SP?
If there are any available, I was wondering what prices and lead-times are for them?
I noticed that the datasheet mentions that there are engineering evaluation samples…
Part Number: ADS1282 Yes, I'm using the ADS1282EVM board, but not the DSP board that it mounts on. I've got my own PCB I've mounted it on.
My question is about getting data out of the ADC. I've been using the info in the data sheet for the…
Part Number: ADS1282 I have a system with 3x ADS1282 ADCs. I need them all to sample at the same instance. They all share a /PWDN, /RESET, and SYNC signals from an MCU. These also all use buffered copies of the same 4.096MHz clock.
They are all powered…
Hello Cole,
many thanks for additional data about LET = 60.4 MeV·cm2 /mg at 85°C and good to know that SBAA222 is going to be updated.
If I cannot receive the complete report [6. Inc, Aeroflex RAD, "SEE Test Report for Texas Instruments ADS1282…
Part Number: ADS1282-SP
dear All,
it is not clear what disruptions are analyzed in the SET section of SBAA222 (SEFI, SET, register SEU’s), and what is not considered even if relevant, for which we don’t have data.
Table 5 is relevant to? …
Part Number: ADS1282 I am unable to get digital data from an ADS1282 ADC.
(CH1: SCLK, CH2: DIN, CH3: DRDY, CH4: DOUT)
I have made sure that PWDN and RESET pins are high. The DRDY output is constantly high.
The ADC ignores the serial clock, and the RDATA…
Part Number: ADS1282 Other Parts Discussed in Thread: OPA4277 , ADS1118 , ADS131M02 , ADS1262 , ADS1256 Hi..
One of my customer is working on high resolution temperature controller & they have considered ADS1282 for their project.
They have used OPA4277…