Part Number: ADS1282 Hello Team, I would like to verify the adc codes for some known input voltages for the testing purpose. As I found from datasheet, maximum differential input would be 2.5v for my case. I supplied 3.3v of the evm board to the AINP1…
Hi Zhe,
The ADS1284 does not have a common mode voltage integration, and neither does the ADS1282. The closest feature I can think of is using the internal MUX to switch to (AVDD-AVSS)/2 through internal resistors, but this is for measuring offset and…
Part Number: ADS1282-SP Other Parts Discussed in Thread: ADS1282 Hello there,
I am currently developing a FPGA design to control and retrieve data from the ADS1282-SP converter. Is there a functional stub or any other module of reference for the articulated…
Part Number: ADS1282 Other Parts Discussed in Thread: REF5025 , I am having trouble calculating the input voltage to the ADS1282. I am using a REF5025 as a voltage reference.
The ADS1282 is connected to a TI TIva TM4C1231D5PMT MCU.
The voltage on the input…
Part Number: ADS1282 Hi Team, seeking some clarification.
Currently trying to read a thermocouple using the ADS1282HPW, but have run into an issue where the adc is outputting in a way that makes it seem like the AINN2 is connected to ground rather than…
Part Number: ADS1282 Hi,
Good Day.
The customer would like to ask about ADS1282 and the possibility of underclocking the ADC.
He needs to check if it is possible to underclock ADS1282 ADC to achieve a final data rate of 100 SPS.
The ADC is working at 250…
Hello Cole,
many thanks for additional data about LET = 60.4 MeV·cm2 /mg at 85°C and good to know that SBAA222 is going to be updated.
If I cannot receive the complete report [6. Inc, Aeroflex RAD, "SEE Test Report for Texas Instruments ADS1282…
Part Number: ADS1282-SP Wondering what CoTS equivalents there are for the ADS1282-SP?
If there are any available, I was wondering what prices and lead-times are for them?
I noticed that the datasheet mentions that there are engineering evaluation samples…
Part Number: ADS1282 Yes, I'm using the ADS1282EVM board, but not the DSP board that it mounts on. I've got my own PCB I've mounted it on.
My question is about getting data out of the ADC. I've been using the info in the data sheet for the…
Part Number: ADS1282 I have a system with 3x ADS1282 ADCs. I need them all to sample at the same instance. They all share a /PWDN, /RESET, and SYNC signals from an MCU. These also all use buffered copies of the same 4.096MHz clock.
They are all powered…