Thank you very much Keith!
Fyi only for those who would refer to this ticket in the future. The Space grade variants of the devices mentioned above are the following:
ADS1282-SP ADC128S102QML-SP LMP2012QML-SP
Art
Part Number: ADS1282 Hi Ti Team,
While surfing the internet I found a research paper "Research on a high-precision and high-resolution seismic wave signal acquisition system" which uses ADS1282 ADC and they are achieving 24 bit noise free count at…
Hi Tsuneharu,
The ADS1282HPW, or the ADS1282-HT, is an Extended Temperature Plastic variant of the ADS1282. I'm not aware of this device being MIL-PRF-38535 qualified.
Might your customer be referring to the ADS1282-SP space-qualified device? If so…
Hello Venkatavel,
Short Summary:
In general, there are a lot of caveats needed to get the performance you’re looking for with the ADS1282. ADS1261 might be a better part for you because the DC performance is a better than the ADS1282.
But if you…
Part Number: ADS1281 Other Parts Discussed in Thread: ADS1282 , ADS1262 , ADS1220 Hi experts,
I've watched videos in 'TI precision labs - ADCs' and benefited from it. But I'm still confused about some parameters of practical ADCs and their usage for my…
Thanks for that Information Richard!
Could you also help determine outgassing data for the part numbers listed below?
• ADS1282-SP
• DAC121S101QML-SP
• DS96F174MQML
• ADC128S102QML-SP
Thanks,
Tyler Barrett
Hi Venkatavel,
Equation 1 in the datasheet is used to convert from SNR to noise RMS and effective resolution. Here is an Excel file that shows this computation:
ADS1282 FIR Noise Performance.xlsx
NOTE: Effective resolution is a DC metric which can be…
Part Number: ADS1282 hello, we plan on using 1 ADS1282 in pulse-sync mode (non-continuous mode). I'm having a hard time understanding the datasheet on how to drive the SYNC pin, or if I even need it.
assuming that CLK is 3.125 MHz and SCLK is 1.5625…
Part Number: ADS1243-HT Other Parts Discussed in Thread: ADS1278-HT , , ADS1282-SP Hi There
I've provisionally selected the ADS1278-HT for my high temperature downhole drilling application, but on closer inspection the gain and offset errors are possible…