Part Number: ADS1294 We are using ADS1294 in a 4-channel ECG application with an STM32F4 MCU. The device is running in RDATAC (continuous conversion) mode. Under normal operation, the 24-bit status word is consistently:
0xC0 0x00 0x00
However, during…
Part Number: ADS1294 In the hardware circuit I designed this time, the MCU and the ADS1294 are powered separately, and it's almost impossible to power them on simultaneously. Furthermore, the MCU has no control over the power supply of the ADS1294; they…
Part Number: ADS1294 Other Parts Discussed in Thread: OPA376 , We are developing a basic EEG acquisition device utilizing the ADS1294. Our front end currently consists of 2 active/ dry electrodes for signal + reference, and one dry electrode to bias through…
Part Number: ADS1294 We are using TI product ADS1294 IPAG in our mobile ECG device. In order to certify it, it is necessary to pass the ESD test according to IEC 60601-1:2005 . On the preliminary test, all the analog ECG input pairs were damaged (lost…
Part Number: ADS1294 We are using TI product ADS1294IPAG in our mobile ECG device. In order to certify it, it is necessary to pass the ESD test according to IEC 60601-1:2005 . On the preliminary test, all the analog ECG input pairs were damaged (lost…
Part Number: ADS1294 Tool/software: Hello,
The manual for ADS129xLow-Power,8-Channel,24-BitAnalogFront-EndforBiopotentialMeasurements includes sample code for RLD Measurement/Setup in section 10.1.1.2 Right Leg Drive.
The code is as follows:
WREG…
Part Number: ADS1294 Other Parts Discussed in Thread: ADS1296 , ADS1296R , Dear Sirs!
It is not clear to me what shall I do with pins
1A, 1B, 1C, 1D, 2A, 2B, 2C, 2D (IN5P - IN8P, IN5N-IN8N) of ADS1294. BGA case.
From one side these channels are…
Part Number: ADS1294 Hello. I have a question about ads1294ic.
1. I am currently designing a contact heart rate measurement system with ADS1294. I would like to inquire about kind of the connectors, types of cables, length of cables, and the material…
Part Number: ADS1294 Tool/software: Hello, I have one question. I was originally used as differential mode, but there are cases that I need to measure the heart rate with one hand.
In the circuit, after removing R158, R163 from the HW point, it was…