Part Number: ADS1296
Hello I am currently using the ADS1296 (6-ch device) for an ECG application and have a question regarding the serial interface...
My master clock is 2.048MHz, I need to sample at 32ksps and I am using only using 3-of-6 available…
Other Parts Discussed in Thread: ADS1296 Hello I am using the ADS1296 with bipolar supplies +/-2.5V. So AVDD = +2.5V, AVSS = -2.5V. There are 2 possible settings for the ADS1296 voltage reference (VREF) in CONFIG register 3 bit 5.
a) If bit 5 is 0 …
Other Parts Discussed in Thread: ADS1296 Hello,
I use the ADS1296 as following:
Internal ref: 2.4V; Analog Vdd: 5V; Digital Vdd = 3.3V; LP mode; 250SPS
I use channel 3.
INN3 = gnd and INP = 1.04V. Input: normal IN.
Either in RDATA and RDATAC…
Other Parts Discussed in Thread: ADS1296 Hello,
I am using ADS1296 to measure the DC output voltage from the Agilent U8002A single output DC power supply.
I have configured the ADS with the following,
Data rate :- 500 sps
Mode :- High Resolution…
I have Lead V wired into CH4. V is routed to IN4P and WCT is routed to IN4N so that V - WCT = Lead V. Lead I(IN2P-IN2N), Lead II (IN3P - IN2N). What does my CH4SET register need to be configured as if I want a gain of 2, 0x20? If so what do my other CHnSET…
Hey Brian,
I delayed (+1sec) a few the ADS1296 init after powering up . Now, when the first SDATAC + delay + RREG ID fails, I re-send the SDATAC + delay + RREG ID many times in a loop. It always pass with a few attempts, usually less than 5.
Best…
Hi Brian,
Ok, I fully respect your advices concerning the scheduling.
The goal was a test of the ADS1296. But I am still confused with some read values so I open a different post to avoid topics mixing.
Best regards
Michel
Other Parts Discussed in Thread: ADS1296 Hi,
I am working on data acquisition device with ADS1296.
In the 24 bit resolution data ADS gives, w hich bit represents a precision of 0.25uV (micro volt) ?
i.e) After getting 24bit data how many right shifts…
Other Parts Discussed in Thread: ADS1296 Hello,
I have a new issue with the ADS1296: I toggle between conversion + read continuous and stop conversion + stop continuous mode and sometimes I have only 0 for all channels data???
I toggle the commands…
Other Parts Discussed in Thread: ADS1296 , ADS1298R , TMS320C5515 Hi,
We have the following design: 1 x ADS1298R and 1 x ADS1296 in daisy-chain (ADS1296 -> ADS1298R) and this is connected to a TMS320C5515 - EVM board.
We have started with the TI medical…