Part Number: ADS131E04 Other Parts Discussed in Thread: ADS131E08 Hello,
I am having a problem with the ADS131E04. Internal oscillator on the device is not working. CLKSEL pin is connected to 3.3 V and CLK to GND. Device does not respond at all. If I…
Part Number: ADS131E04 Some times after power interruptions Controller not able to read Device ID. Normally i am getting "0xD0". But after these mentioned times it is reading "0x00". Supply is stable during this reading time. SPI frequency = 8MHz…
Part Number: ADS131E04 Other Parts Discussed in Thread: ADS131E08EVM-PDK
Hello, everyone,
I would like to read out the ADS131E04 with an Arduino Due via SPI. Unfortunately, I have little previous experience, and this is my first project with an SPI communication…
Part Number: ADS131E04 Tool/software: TI C/C++ Compiler Hi,
I'm dealing with this ADC, and I'm using STM32 MCU as the hist CPU, my problem is that I could not configure the Device so I could connect and read registers or converted data from this ADC,…
Hi Angel,
Thank you for your suggestion.
1. In some applications, Neutral will be available. We can measure either only Phase to phase Voltage or only Phase to neutral voltage or both can be measured, right? So, Neutral is not mandatory for this circuit…
Part Number: ADS131E04 Hello,
my customer is currently working on a project and he plans to use the ADS131E04. however he has a question about the current consumption of the device specially for Analog VDD/VSS lines. He will be using 3 ADC chips daisy connected…
Part Number: ADS131E04 Other Parts Discussed in Thread: ADS131A04 , ADS131E08 , ADS131M04 , INA826 , ADS1292 , ADS1291 , INA828 , OPA2188 , Hello
I want use ADS131 in my project; i found there is 3 versions E , A and M ; What are the main diffirences ?
I read…
Part Number: ADS131E04 Other Parts Discussed in Thread: OPA333 Hi there,
we are plannng to use the ADS131E0x or A0x.
We have a single ended signal between -4V to +4V to convert.
To bring this signal to fully-differential adc-input, we will use a difference…
Part Number: Hello ,
I have a question that mixed my mind and i am not sure about it , i hope you help me to solve it
I use ADS131 to read an anlalog signal at 2kHZ sampling ; the ADS132 has an RC input filter about 10KHZ ;
but I need to decimenate…
Part Number: ADS131E04 Other Parts Discussed in Thread: ADS8861 , , ADS8363 , ADS8556 , ADS8910B Hi team,
My customer Qunling is working on a project. In this project, they get four signal need to be sampled, one high speed signal, grid current、voltage、one…