Part Number: ADS131E04 Hi all
My customer is using the ADS131E04 with an external reference and he has this question (referring to Figure 28 in the Datasheet):
When the internal reference-buffer is in shutdown, what happens to R2/R3?
Is there 50kOhm between…
Mattia,
Thanks for posting back with an explanation of the solution. I'm glad that you were able to figure out that problem.
If you have any other questions on the ADS131E04, feel free to post back to this E2E forum!
Joseph Wu
Part Number: ADS131E04 Other Parts Discussed in Thread: ADS131E08 , ADS130E08EVM-PDK , ADS130E08 Tool/software: Code Composer Studio hello;
Could somebody send me the zip file of ADS131e08 and the password
to use it in my new project. Thank you.
touatinasri2…
Part Number: ADS131E04 Other Parts Discussed in Thread: ADS131A04 , Hi Sir
May Ads131 can replace AD9629?
customer use in FFT function.
data rate about 20~30Kbps/per 1chennal , total 4channel. customer request Automotive rating.
May you have suggestion…
Part Number: ADS131E04 Dear Team,
our customer would like to use the ADS131E04 and has a question about the propagation Delay between CLK to DRDY.
Do you have any value for this?
Thanks and best regards Martin
Part Number: ADS131E04 Customer was working on ADS131E04IPAG, they have noticed that in the Pin Configuration and Functions diagram & Pin Functions table (page No. 4-6 of the datasheet), Signal at Pin Number 60-64 is given as OPAMPP, OPAMPN,NC, OPAMPOUT…
Hello Roy, Thanks for your post. I assuming that you're using the ADS131A04, not the ADS131E04? M0, M1, M2 do not exist on the ADS131E04. I've corrected your original post. By "offen," do you mean that the M1 pin is floating? M1 = floating…
Part Number: ADS131E04 Hello!
I am using ADS131E04 to sample three devices. I am counting on the fact that with a 2.048 MHz external clock the sample rate should be exactly 4000 Hz, with the same accuracy.
Is that true, or should I expect some differences…
Hi TATSU Numa,
The customer might consider using a simultaneous sampling ADC then, if they want to measure many channels in 75us
For example, the ADS131M04 or ADS131E04 could be good options. These devices have 4 ADCs in each package, which means there…
Part Number: ADS131E04 Hi Team,
I have a question about the ADS131E04. Could you help on this question?
Customer tested Power-up timing as follows.
Power ON ---> Wait of 300ms ---> Ext Clock input ---> Wait of 100ms ---> Reset of 5us ---> Wait…