Part Number: ADS131E06
Hi team,
My customer will use ADS131E06 for his application and he is adjusting timing of RESET after PoR.
Although he thought VCAP1 would be charged immediately after power-up of supplies, there is about 400ms delay for start…
Part Number: ADS131E06 Other Parts Discussed in Thread: ADS131M06
The data sheet has some conflicting information, so I was wondering if you would be able to clarify:
https://www.ti.com/lit/ds/symlink/ads131m06.pdf?ts=1610052930617&ref_url=https%253A…
Part Number: ADS131E06 Hi support team.
I have the inquiry from my customer regarding PSRR spec.
Does the PSRR spec in datasheet apply all power supplies(AVDD,DVDD)?
Could you give me the information?
Best regards,
Higa
Part Number: ADS131E06 Hi,
I am using an ADS131E06 converter configured for 4V internal reference and it is powerd by +-2.5V supply. The input signal normally is between +-4V differential voltage symmetrically to Vss.
Sometimes I get strange readings…
Part Number: ADS131E06 Hi support team.
Is a low noise LDO needed for a DVDD?
My customer would like to know if the noise to DVDD affects the conversion error.
Could you please provide PSRR vs frequency data regarding DVDD?
Best regards,
Higa
Part Number: ADS131E06 Other Parts Discussed in Thread: ADS124S08 , ADS1220 Hi,
I'm looking for suitable ADC for PT100/PT1000 (4-wire) input interface.
Which ADC is recommended (ADS131E06IPAG, ADS124S08 or any other new ADC)?
Can you share any available…
Part Number: ADS131E06 Customer meet ADS131E06 issue. They report they met ADS131E06 register write failure issue, failure rate 20%.
If the configuration of ADS131E06 fails, it will not follow ADS131E06, nor will it follow MCU. This is random. If they…
Part Number: ADS131E06 Tool/software: Code Composer Studio hi
im working with analog digital converter ADS131E06 i want to know if i should powered ON device then powered ON reference voltage, or the opposite.
Or I am free in the choice, i means who powred…
Part Number: ADS131E06 Hi, I was wondering if there is a source code I can see in order to communicate with the ADC.
I have been implementing SPI communication from FPGA, but the ADC do not answer any command.
Thanks
Part Number: ADS131E06 Hi All,
Good Morning !
I need some clarification on ADS131e06 ADC chip regarding the usage of DRDY pin. I actually gone through the data sheet several times, but still it is bit confusing to me.
I have following queries;
1. Can…