Part Number: ADS131M08 Other Parts Discussed in Thread: ADS131E08 Hi team,
May I know if the SPI software drive parts are the same for ADS131M08 and ADS131E08 ?
If the customer has designed the ADS131M08 and wants to change to the ADS131E08 later, is the…
Part Number: ADS131E08S Hello, I'm using 74HC4051D to mux 5 analog signals into one single pin of the ADS131E08S. I've tested multiplexing each signal individually and measuring the output with a Digital Multimeter and it outputs the corresponding analog…
Part Number: ADS131E08 Hi team,
In datasheet of ads131e08, it requires 4tclk min time for Tsccs. Customer used 2.048MHz clock and the minimum time of Tsccs should be 1952ns. But in actual system, the Tsccs time is only 100ns. Could you pls help to clarify…
Part Number: ADS131E08 Hello, I’ve designed a custom board which uses the ADS131E08 for measuring simultaneous current and voltage measurements. Unfortunately I am running into issues, the DVDD which is attached to 3.3V rail (LDO on board) is effectively…
Part Number: ADS131E08 Hi Ti, i am trying to set config1 register to 0x90 to make ADC to run at 64ksps Data rate. But still ADC is running at 32ksps. I have tried 8,16,32ksps those looks to be fine DRDY is coming as expected. But when i tried to run ADC…
Part Number: ADS131E08 Hi, I am using ADS131E08IPAGR in one of the designs and need information on power budgetary for this part.
Please refer below specs for application.
AVDD = 5V
DVDD = 3.3V
All the analog input pins are used.
Internal op amp is not…
Part Number: ADS131E08S Hi,
I am using the ADS131E08SPAGR and our setup has the following power-up sequence (as can be seen in the image): First DVDD powers up to 3.3V then 8ms after AVDD & AVDD1 power up to 2.5V and AVSS & AVSS1 to -2.5V.
I wanted…
Part Number: ADS131E08 The internal leadframe pattern between our provide parts (D/C:2316) and customer reference parts (D/C:2315) has little inconsistent (see the picture -parts corner with red circle area), we replied that this maybe caused by different…
Part Number: ADS131E08 Other Parts Discussed in Thread: ADS131M08
Hi,
I'm running the chip in continuous mode and saw that sometimes when I poll the data via SPI, the data ready flag will spike, indicating that a new conversion result is ready. One of…