Mr Anbarani -
Yes the ADS1298 is targeted at ECG applications, but we have had folks use it for EMG purposes. In the software, the data is collected and displayed in time domain, histogram, and FFT that are independent of the ECG display. So you could…
Niranjan -
The device is capable of being used as a generic ADC, you just need to change some of the default settings on the EVM.
Take a look at the schematic in the user guide (end of http://www.ti.com/lit/ug/sbau171c/sbau171c.pdf ). Using the D15…
Part Number: ADS131M08EVM Hii.
It looks like the EVM GUI does provide continuous save to file for samples , but only in small 16384KB files.
Is this expected ?
Pierre
Hello!
Looking at the Table7 of the IC datasheet, I'm trying to figure out what's the reason behind settling time for 64ksps and 32ksps modes being, accordingly, 152 and 296 fCLK cycles.
I do understand there's, apparently, 4 tCLK delay to startup…
Other Parts Discussed in Thread: ADS1256 , ADS1248 Matt,
Thanks.
May I also ask about ADS1256?
I am confused how to understand table 14 in the datasheet.
What is the difference of data rate and cycling throughput?
And, how should I understand…
Hi Inge,
Data rate in the ADS131E0x is defined by clock frequency and the DR[2:0]bits in the CONFIG1(Configuration Register 1)
DataRate = f clk /2/ K ? where K is value which is determined by DR[2:0].
DR{2:0] = 000 K=16 DR{2:0] = 001 K=32 DR{2:0…
Other Parts Discussed in Thread: ADS1209 , ADS124S08 New users to E2E
If you are new to the support forum, please take some time to read the E2E community guidelines and tasks specifically related to E2E and resource guides listed below:
Search…
Part Number: ADS130E08 ADC Reset pin going low for 2uS when there is a disturbance (Ringing Noise) on Main Power supply (15V). May I know TI recommendation to fix this issue?
Hi,
I am running this EVM and find out the sampling rate is only available up to 16KSPS for the EVM. Is any way to test 32K and 64KSPS with this board?
Thanks,
Ming