Part Number: ADS131E08 Other Parts Discussed in Thread: ADS131M08
Hi,
I'm running the chip in continuous mode and saw that sometimes when I poll the data via SPI, the data ready flag will spike, indicating that a new conversion result is ready. One of…
Part Number: ADS131E08 Other Parts Discussed in Thread: TIDA-010086 , ADS131M08 , REF5025 Hi DCC Experts
Problem: There is a current fluctuation when using TI ADS131E08 to measure 4ch voltage and current. You can see the phenomenon as below.
This…
Part Number: ADS131E08 Hi team,
Customer test the EVM and internal short input. The noise result is shown as below. Vpp is much larger than 6.6 times Vrms. Could you pls help me understand the reason? And any suggestion that can improve Vpp of noise? …
Hi Rayna,
One more thing I forgot in my previous post. An Offset voltage is seen on each channel, so it's good for the customer to do offset and gain calibration.
Best regards,
Dale
Part Number: ADS131E08 Hi, can I check what is the full scale range of the ADS131E08 when AVDD = 5V and AVSS = 0V and a PGA of 12 is applied?
Based on the datasheet, the differential input voltage = +-VREF/Gain.
In which case, for VREF = 2.5V and Gain…
Part Number: ADS131E08S Hi Team,
I am working with your ADS131E08S and have some questions on the device below.
1) Are the differential inputs on these devices bipolar?
2) If so, can the device be configured to have the negative differential input grounded…
Part Number: ADS131E08 Other Parts Discussed in Thread: ADS1278 Checking he datasheet, we realized the ENOB to this PN working with 16ksps is 17bit and our application needs at least 20bits.
Do you know an alternative part with at least six simultaneous…
Part Number: ADS131E08S Other Parts Discussed in Thread: ADS131E08 , Hi team,
In datasheet of ADS131E08, Equation 1 in 8.1 describe the formula of ENOB.
In datasheet of ADS131E08S, Equation 1 in 8.1 describe the formula of effective resolution.
Could you…
Part Number: ADS131E08 Hello, I am working with ADS131E08 ADC. I have done ADC interface with one controller and I am using FreeRTOS. ADC initialization is done before RTOS start scheduler. Where I have two task, one task is for simple print massage other…
Part Number: ADS131E08 My interest on measuring 40th harmonics when my fundamental frequency is 60hz , what I understood is due to SINC filter signal attenuation is high at 2.5 KHz input signal (Harmonics signal) , I would like to understand the signal…