Part Number: ADS131M02 Hi,
The ADS131M02 datasheet states in the absolute maximum ratings section:
AINxP, AINxN: max AVDD + 0.3V
continuous, all pins except power supply pins: max -+10mA
For the device to be damaged, do both of these must…
Part Number: ADS131M02 Hi,
The ADS131M02 datasheet states Input Bias Current = 0.6uA typ for gain < 8, and 0.2uA typ for gain >= 8.
Where the "typical" values above are for room temperature.
What is the temperature drift of the bias current? or…
Part Number: ADS131M02 When issuing a register read command via SPI, the chip sometimes replies as expected, but sometimes skips the CRC frame. This means the response doesn't arrive at the expected frame. Is this behaviour known and expected?
Here…
Part Number: ADS131M02 Other Parts Discussed in Thread: ADS131M03 , Hello,I am working with the ADS131M03 in a new project and have encountered challenges related to its input impedance, which are affecting our measurement accuracy.
Our circuit has…
Part Number: ADS131M02 Hi team,
Customer is tesing ADS131M02, they get several inquiries, could you help share comments?
1. When the ADS131M02 finishes conversion, the DRDY pin goes low, generating a falling edge and triggering an interrupt to read…
Part Number: ADS131M02 My team was curious what happens when the ADS131M02 analog input exceeds the AVDD-1.8 when operating at a gain greater than or equal to 8. Would the device be damaged?
Part Number: ADS131M02 Other Parts Discussed in Thread: ADS1235 , ADS1234 , ADS1232 Hello,
I am referring ADS131M02 and trying to understand what noise free resolution I can obtain assuming I will be using two layer PCB.
My application is similar…
Part Number: ADS131M02 We are currently using the ADS131M02QPWRQ1 for BMS voltage and current monitoring.We observed that the ADS131M02Q1 emulation/evaluation board uses the SIT8924BA-22-33E-8.192000G oscillator as the reference clock for the ADC.Since…
Part Number: ADS131M02
I am currently testing the ADS131M02 with a strain gauge. The ADC is soldered on a demo board and connected to my microcontroller via jumper wires.
I have observed the following issue:
After each power cycle (power off…
Part Number: ADS131M02 Tool/software: Hi, I am having problems modifying the gain setting registers on the ADS131M02. The ADC works on default settings as I have successful communication via SPI with a raspberrypi 5, but the problem arises when I try…