Part Number: ADS131M02 Other Parts Discussed in Thread: ADS124S06 , ADS131M08 , ADS124S08 , ADS1248 , ADS1247 , ADS1261 , ADS1260 , ADS1220 , ADS122C04 TI has some ADCs (such as the ADS124S06 ) that are very well suited to ratiometrically measuring RTDs (4 wire…
Part Number: ADS131M02 We have the mikroe adc 15 board for testing and after setting everything up I started noticting only the irst readings were valid. After ~1.96seconds the board resets and we get 0xFF22 indicating a succesful reset. This seems to be…
Part Number: ADS131M02 Other Parts Discussed in Thread: ADS131M04 , Hi
If we done the fine tune on ADS131M02. can we use the same register settings on ADS131M04 to got the same performance?
Part Number: ADS131M02 Other Parts Discussed in Thread: ADS131M04 , ADS131M08EVM , , ADS131M04EVM , ADS131M08 Hi team
Does it have EVM? Or, I can use ADS131M04/06/08EVM? Which part is the most similar to M02?
Thanks
Part Number: ADS131M02
Hello.
I'm using ADS131M02 to convert photo diode's value with raspberry pi 4B+.
When read CLOCK register, Response data is 0x030E. That is default value.
And write CLOCK register that data is 0x030A, Response data is…
Part Number: ADS131M02 Other Parts Discussed in Thread: ADS131A04EVM , ADS131A04 , ADS131M04EVM Hi team,
This is a new design in my customer. It is the first time for them to use ADS131M02IPW. They found DRDY output a periodic pulse with duration is about…
Part Number: ADS131M02 Hi,
Customer is encountering problem with ADS131M02, below is the details.
"The ads131m02 chip can read the register data normally, but it cannot be written
VCCS_SPI_RST_LOW; vTaskDelay(5); //delay 5ms VCCS_SPI_RST_HIG…
Hello ACGUY,
The DRDYn behavior can change depending on when conversion data is read from the device. In the case where a new conversion is completed while the previous conversion is still being read, the DRDYn pulse is internally gated and blocked from…
Part Number: ADS131M02 Hi Team,
I would like to know a suitable EXTERNAL CLOCK SOURCE.
(I need around 16bit resolution and data rate is TBD.)
I can find “Table 7-2. Dynamic Range (Effective Resolution) at TA = 25°C” in the datasheet.…
Part Number: ADS131M02 In the ADS131M02 datasheet, the frequency of the clock source is provided based on different power mode. Could you please help check whether it can use the clock from the MCU, like C2000? Is 8.192MHz for High-resolution mode necessary…