Other Parts Discussed in Thread: ADS131M08 Hi,
Actual I am developing an application where I required to use ADS131m08 so I have few questions
1. if we are using a separate controller like STM32 or any other do we need to give digital clkin signal if…
Part Number: ADS131M08 Other Parts Discussed in Thread: TMS570LC4357 I am working on interfacing with two ADS131M08 devices using a TMS570lc4357 (SPI1) and having some odd behavior on the MISO lines. The design is configured so that it uses MibSPI parallel…
Part Number: ADS131M08-Q1 Other Parts Discussed in Thread: ADS131M08 Hello,
We are trying to achieve a wider FSR with the ADS131M08-Q1. We see that in the datasheet, the maximum recommended voltage for REFIN is 1.3V, though the pin is rated to AVVD + 0…
Part Number: ADS131M08-Q1 Other Parts Discussed in Thread: ADS131M08 Hi team,
The attachment is the schematic diagram of the customer's ADS131M08. Please help to check, the chip part, the customer's library is not completed, and a 32PIN is used instead…
Part Number: ADS131M08
Hello,
I noticed the following in the datasheet:
Can you elaborate on the reason why the Master Clock needs to be synchronous with the SPI interface clock (SCLK)? It does not appear that the EVM is following this requirement…
Part Number: ADS131M08 Other Parts Discussed in Thread: LM27762 HELLO EVERYBODY. I HAVE A PROJECT TO READ 4 LOAD CELLS AND I AM USING THE ADS131M08 IC WHICH HAS 16 DIFFERENTIAL CHANNELS. I AM CONNECTING 4 2mV/V LOAD CELLS WITH 10V EXCITATION. I AM USING…
Part Number: ADS131M08 I narrowed down my search for 8-channel Delta-Sigma ADCs to your ADS131M08IRSNR or Microchip's MCP3914A1-E/MV for a new project that we're calling the Fast Response Probe or FRP. Since both companies use different methods…
Part Number: ADS131M08
Hello everyone,
I have a project consisting of making an ADC main board with a raspeberry PI4B which will allow me to measure differential voltages from a analog accelerometer sensor on remote micro-boards.
The fact I cannot use…
Part Number: ADS131M08 Hi,
Good Day.
I am looking at the ADS131M08, trying to understand if that can read all 8 channel differential signal at 24bit each at 32kSPS.
And also for its SPI link, if I want to have all these data out (32*1024*sps*24bit*8channel…