Part Number: ADS1675 Hi Experts,
I am unable to find the Junction-to-Board thermal coefficient in C/W for ADS1675 in the available datasheet. Can you help?
Regards,
Marvin
Part Number: ADS1675 Other Parts Discussed in Thread: TXU0101 Tool/software: Hi we have a custom board with the ADS1675 and we observe a strange issue: Sometimes two samples samples in the data stream is shifted. One sample is shifted left and the following…
Part Number: ADS1675 I am working on a design with 16 x ADS1675 operating in synchronization. What is the CLK to SCLK delay , TLCLKSCLK, when all ADCs are running on the same voltage, 3.0V +/-1%, and all are operrating at the same temperature, between…
Part Number: ADS1675 Other Parts Discussed in Thread: LP2992 , TPS82130 Tool/software: We use the ADS1675 in one of our products which is already in mass production. Normally it works fine. But roughly every 100 th device we see a strange behavior.
…
Part Number: ADS1675 Hi Support Team,
Correct me if I'm wrong, but the only way to have 2MSPS with ADS1675 is with the following settings:
Fclk = 16 MHz
DRATE = 101 => Fclk/8 = 2MSPS
With DRDY timing = 1/2MSPS = 0.5 us
and Fsclk = 16Mhz x 3…
Part Number: ADS1675 I would like a copy of the ads1675ref-plug-in-1.0.0.exe in whatever version. I'm trying to use the ADC pro software to control my ADS1675REF board.
I believe the software was on the website a couple of moths ago, but it was taken…
Part Number: ADS1675 I'm in the process of moving the ADS1675 off of the Opal Kelly 3010 to the Xilinux AC701 and was wondering if TI has updated their policy on re-releasing the FPGA source code?
It was once available on the ftp site which has shutdown…
Part Number: ADS1675 It is not clear in the datasheet but could you please confirm:
Data Rate
Min f_clk
4 MSPS
32 Mhz
2 MSPS
16 Mhz
1 MSPS
8 Mhz
I have configured the ADS1675 for CMOS and therefore I am limited…