Part Number: ADS1675 Hi Sir, When I use ads1675,the OTRA pin is connected to the ground through a resistor and LED light, The LED lights keep flashing after the power on, The measured input level of AINP and AINN is about 2.5V. Even if the voltage of the…
Part Number: ADS1675 Hello,
is there any source code related to the ADS1675? I could find different threads but non with the source code. May someone can email me?
One technical question in addition: is the vhdl implementation alywas with two clock domains…
Part Number: ADS1675 Hello,
I am using the ADS1675 in WIDE-BANDWIDTH FILTER mode. I set the START PIN to high for continuous samp. I can see the DRDY pulse and the date out is correct. But , when outside of the board have EMI NOISE such as ESD in the…
Part Number: ADS1675REF Hi,
I am trying to resolve an offset issue I am seeing on the ADS1675REF eval board:
The inputs on ADS1675REF are set up for single-ended, 0-5V input range. For the offset test -IN grounded (+IN = 2.5V, R8 = short and -IN = 0V…
Part Number: ADS1675 Hallo,i'm using the ADS1675. I will adapt the Input Stage.
I want to know the Input Impedance of +/-AN and the Thermal drift.
Maybe you can send me an Schematic of the Input Stage.
Thanks
Part Number: ADS1675 Hallo,
Can you tell me how the ADS1675 behaves when the maximum temperature is exceeded? which parameters change after the maximum temperature is exceeded. The point is that once the maximum temperature is exceeded, the temperature…
Part Number: ADS1675 Hello Keith,
I am observing an undocumented behavior of ADS1675. There is sometimes a spike on DRDY near the second falling edge of CLK after applying START. The duration of the spike is approx. 1/3 of Tclk. The length of a real DRDY…
Part Number: ADS1675 Other Parts Discussed in Thread: SN74AUC1G74 Hello,
I am debugging a DAQ-system consisting of four ADS1675 that are expected to sample and output data simultaneously but do not. I measure deviations in arrival time of DRDY of around…
Part Number: ADS1675 Hello,
My customer wants thermal resistance value of ADS1675 for the thermal simulation.
Could you please provide the thermal resistance value?
Regards,
Itoh
Part Number: ADS1675REF Hello. I search the VHDL Code for your ADS1675REF Board, to make some modifikation. Can you send me this at my Email please. Thank you and best regards. Juergen Dederichs