Part Number: ADS4122 Other Parts Discussed in Thread: THS4551 , , THS4511 , ADS5500 , LMH6553 Hello,
Our customer consider to use THS4551 and ADS4122 combination.
Here is concern that is ABS input voltage range of ADS4122's INP, INM pin which is AVDD + 0…
Part Number: ADS4122 Other Parts Discussed in Thread: ADS4142 , ADS4125 , ADS4145 Hi,
ADS4122 data sheet (SBAS 520 C) page 13 Analog Power ADS4122, ADS4142 (125 MSPS): 112 mW It is stipulated in.
The ADS4122 and ADS4142 are specified with 65MSPS. (page4 5…
Part Number: ADS4122 Hi, Please tell me about setting with serial communication setting method
Q1. In the data sheet page7 SCLK "When RESET is high, SCLK has no function and must be tied to ground." It has been described as. However, at the timing…
Part Number: ADS4122 Other Parts Discussed in Thread: THS4541 , TIDA-00942 , OPA656 Hi all,
I am working on a project in which I need to sample and convert a 1.5MHz signal. I was hoping to find a microcontroller with a built-in fast enough ADC for this…
Other Parts Discussed in Thread: ADS4122 i want to use multiple ADS4122 into a multiple channel simultaneous sampling system. But I can't find a pin or a register to synchronize the samples of mulitiple ADS4122. So who can offer a method for this simultaneous…
Part Number: ADS5296A Other Parts Discussed in Thread: ADS4122 , Hi,
I will using LVDS clock driver to drive the clock input of the ADS5296A and ADS4122.
in the DS of ADS5296A I find the followed:
The answer to the same question for the ADS4122:
Pls…
Hi,
My customer measures the analog input-pin voltage on the condition that analog input-pin is open.
Then there is the noise synchronized sampling clock.
The waveform is following;
It is mentioned about RCR filter on the figure 105. of the datasheet…
Other Parts Discussed in Thread: ADS4122 , TMS320C6748 Hi,
I am thinking of interfacing ADS4122 to TMS320C6748 DSP for an IF application. It is desirable to sample at about 20~25MHz, 12bit.
The data will be sampled at 20MHz, continuously stream. If we…
Hi,
My customer is troubled that amplitude of the glitch is large after the aperture delay.
Please refer following the waveform.
They tried to add the filter(50Ω and 3.3pF), however there is no improving.
Could you please introduce how to improve…
Part Number: ADS4222 Other Parts Discussed in Thread: ADS4122 , Hello, customer needs to sample 65MSPS, 14bit and is looking for interfacing to a processor. Do we have any Sitara reference design?
Regards, Holger