Part Number: ADS4222
Hello,
I am using 2 pcs ADS4222 to achieve 4 channels ADC as oscilloscope.
But How to synchronize the sampling for these 4 channels?
Part Number: ADS4222 Hello,
Need your help to review the schematic.
1) The application is for measure voltage from u0adc_in or u1adc_in from -100V to 100V. This application is likely an oscilloscope.
2) Sample rate of adc is 50M/s
3) U18 is LVDS clock…
Part Number: ADS4222 Other Parts Discussed in Thread: CDCE72010 Hello,
I am using 1.8V CMOS single end clock to drive ADS4222 clock input.
As CLK_M is connected to VCM (0.95V), should it make CLK_P will exceed 1.8V? Any risk?
Part Number: ADS4222
Hello,
Look at datasheet and lib from TI website.
It seems all the vias in pad are opened in soldermask layer.
From my experience, such via should be covered by soldermask green oil to avoid solder paste in vias.
Could you check…
Part Number: ADS4222
Hello,
I am using LVDS input as clock input for pin 25 and 26.
For better layout reason, I would like to exchange pin 25 and 26 routing. ( CLK- connected pin 25 CLKP, CLK+ connected pin 26 CLKM)
I suppose it also should work when…
Part Number: ADS4222 Other Parts Discussed in Thread: ADS4122 , Hello, customer needs to sample 65MSPS, 14bit and is looking for interfacing to a processor. Do we have any Sitara reference design?
Regards, Holger
Part Number: ADS4222
Hello,
I just see it's recommended to use differential input for best performance.
But if I use single end CMOS clock input, how to make it precisely calculate the reduced performance?
Then I can decided to use it or not.
Part Number: ADS4222
The datasheet requires in serial resistor for CMOS interface to FPGA. how about the value? 10ohm ok?
1) interface of data output
2) interface of spi