Part Number: ADS4222 Other Parts Discussed in Thread: THS4500 ,
Hi,
Please suggest the front end circuit to connect ADS4222,
Currently designing an custom board in which the single ended pulse signal has to be isolated.
The Pulse duration is 1us to 6us…
Part Number: ADS4222 Other Parts Discussed in Thread: THS4509 , Hi,
I want to use ADS4222 for digitizing sensor signal which ranges from 0.9V to 1.8V.
The sensor can drive load of 1K and above. The bandwidth of the input signal is from DC upto 20 MHz. …
Part Number: ADS4222 Other Parts Discussed in Thread: ADC12DL040 , ADC3222 Hi All
My customer is searching high speed A/D Converter that is compatible following specs.
(1) Dual and Simultaneous Sampling (2) Resolution : over 12bit (3) Sampling Rate : over…
Part Number: ADS4222 Other Parts Discussed in Thread: CDCLVD2102 , CDCLVD1213 , CDCLVD1204 Hi Team,
From our ADS4222 datasheet,
Customer is looking for a clock buffer to work with it. They will operate this device at highest sampling rate.
I have 3 quick…
Venu,
I would suggest looking at the ADS42xx family of data converter (12/14 bit, 65/125 MSPS). These are LVDS output devices. The maximum input swing is 2Vpp centered around a 0.95V common mode. Most of our converters will have a common max input swing…
Part Number: ADS4222EVM Other Parts Discussed in Thread: ADS4222 Hi Experts, May I ask if you can please provide the schematic of the ADS4222EVM (LVDS) board?
Our customer downloaded the schematic of ADS4222EVM from here ( ADS42XX_58C28EVM DesignPkg (Rev. B…
Hi Xiaoqiang,
the THS4551 input voltage should be limited to 0V and +1.8V, actually.
Have you thought about using a tranformer, as recommended in the datasheet of ADS4222? Even the ADS4222 EVM has a transfomer at the input.
Kai
Part Number: CDCE6214 Other Parts Discussed in Thread: ADS4222
Hello,
Below circuit was used to provide clock to FPGA and ADS4222.
And FPGA will use I2C to config this clock setting.
What's the initial clock output of below 5 channels before FPGA start…