Other Parts Discussed in Thread: ADS4242 I have following two doubts regarding performance of ADS4242
In the datasheet of ADS4242 typical value of VCM is given as 0.95V. What is Max and min value of VCM for 2Vp-p input level without degradation of…
Other Parts Discussed in Thread: THS4509 , ADS4242 I am using THS4509 to drive ADS4242. I have following doubts about this combination.
On page 9 of the datasheet output VCM of ADC is mentioned as 0.95V
on the page 80 of the datasheet it is mentioned…
Part Number: TMS320C6748 Other Parts Discussed in Thread: ADS4242 Dear Champs,
My customer developed C6748 custom board by connecting ADS4242 ADC in upp port.
In their test, they found Phase difference between 2ch inputs even when they input same…
Part Number: TMS320C6748 Other Parts Discussed in Thread: ADS4242 Dear Champs,
My customer found wrong data from the upp when they generated test pattern in the ADC which increase data by 1, and ADC is ADS4242 is connected to upp.
But, they found…
Venu,
I would suggest looking at the ADS42xx family of data converter (12/14 bit, 65/125 MSPS). These are LVDS output devices. The maximum input swing is 2Vpp centered around a 0.95V common mode. Most of our converters will have a common max input swing…
Hi,
There is no such a device as ADS42P42. If you meant ADS4242, SPI clock comes from FTDI USB chip. You'll not need a sampling clock for SPI configuration, but the basic functionality of ADC including test pattern will not work without a sampling clock…