Part Number: ADS4245 Hi,
I have a question regarding to the ADS4245 digital inputs : CTRL[1:3],SCLK,SEN,RESET-
Naturally, since they defined has digital pins- – I would connect them to the digital reference rail - DRVDD.
But in the EVB these pins…
Part Number: ADS4245-EP Other Parts Discussed in Thread: ADS4245 Hi all,
We are using ADS4245 EP in our design and you can see the below schematic related to the ADC portion of the design. R268 is not mount, CTRL1 is tied to a power down signal. We are…
Part Number: ADS4245EVM Other Parts Discussed in Thread: ADS4245 Hello,
My customer wants to test the ADS4245EVM after purchasing it.
The ADS4245EVM webpage on TI.com states that it is directly compatible with the TSW1400EVM and TSW1405EVM, but they cannot…
Part Number: ADS4245 Will the part be damaged if the input signals are present when the ADS4245 is not powered?
I see that it has protection diodes and that is why I am asking the question.
I did not see this anywhere in the forums.
Thanks for your help…
Part Number: ADS4245 Other Parts Discussed in Thread: LMK04000 Hi,
The ADS4245 will be connected to Altera FPGA in LVDS mode (similar to what you demonstrates in http://www.ti.com/lit/ug/slaa545/slaa545.pdf )
The FPGA (CycloneV E) LVDS transceiver are…
Other Parts Discussed in Thread: ADS4245-EP Hi,
One of my customers is using the ADS4245-EP in a parallel CMOS output format at 15Msps. The datasheet mentions the output setup and hold time on the parallel interface starting from 65Msps in Table 3 on page…
Other Parts Discussed in Thread: ADS4245-EP , ADS4245 Hi sir,
I am using a ADS4245-EP and i have problems... With my 6 first prototypes, 3 are working well and 3 other doesn't work...
First 6 prototypes have AD4245-EP from same batch.
The problem seem…
Other Parts Discussed in Thread: ADS4245 Current consumed by ADS4245 in parallel CMOS 2'complement mode is very high(420milliAmps). typical current given is 230mA maximum. I am working at 15MSPS speed and using single channel by powering down other channel…