Part Number: ADS42LB49 Can the ADS42LB49 be configured in QDR mode to allow the DAFrame and DAClock to be used in the clocking for the B Channel Data?
Thank you for the help,
David
Part Number: ADS42LB49
Hi Team,
I have TI "ADS42LBx9 14- and 16-Bit, 250-MSPS, Analog-to-Digital Converters" chip eval board with FMC connector. I want to program the configuration of it by using ZedBoard FPGA device. I used earlier AD9361/64 device…
Part Number: ADS42LB49 Other Parts Discussed in Thread: LMH6552
hi expert.
ADC works in AC couple mode. schematic as follows, U1 represents LMH6552, and U2 represnets ADS42LB49.
FFT plot measured in above C1 blue circle point by Agilent spectrum analyzer…
Part Number: ADS42LB49 Other Parts Discussed in Thread: TSW14DL3200EVM Hi Experts, Our customer recently developed a data acquisition card with ADS42LB49, using kinetex7 FPGA (xc7k325t-2ffg900) of Xilinx as the main control unit. He want to ask if there…
Part Number: ADS42LB49 Other Parts Discussed in Thread: LMH5401 , LMH6552 hi expert,
i'm using ADS42LB49 to sample high speed ac signal, but at the same time need to sample dc voltage combined with high speed ac signal.
from datasheet, it recommends…
Part Number: ADS42LB49 hi,
in my dsign. ADS42lb49 works in DDR mode, and LVDS data signal has some problem when sampling a 200mv square signal. as ADS42lb49 input Vpp max is 2V, so when 200mv signal input to INAP/M, DA12P/M should keep 0, but i captured…
Part Number: ADS42LB49 Other Parts Discussed in Thread: ADS5500 , , CDCV304 , CDCE62002 Hello,
I am performing 512 point FFT on both adcs with sampling rate 100 MHz
ADS5500 using differential clock source
ADS42LB49 using cmos clock source
The input signal…
Part Number: ADS42LB49 Hello,
I am using ADS42LB49 at 100 MHz sampling rate and an FPGA to perform FFT.
The power spectrum does not look uniform when sweeping a signal from 0 to Fs/2 on the input.
It is lower on the low end and the high end of the spectrum…
Part Number: ADS42LB49 Hello,
I am using channel A with sampling rate of 200 MHz and in DDR mode, I want to power down channel B since I am not using it and noticed the following in the datasheet:
Does this mean I cannot power down channel B when using…
Part Number: ADS42LB49 Other Parts Discussed in Thread: CDCE62002 Hello,
I am working on a design and planning to use ADS42LB49 at 200 MHz sampling rate.
I though about using CDCE62002 as clock source, but the jitter seems a bit high for the ADC?
Is…