Part Number: ADS5263 Hi TI,
Could you please provide the quotation, availability, and lead time for the below components?
Please include:
Unit Price
MOQ (Minimum Order Quantity)
Available Stock
Lead Time
Manufacturer Name
Active part…
Part Number: ADS5263 Tool/software: I currently am exploring design options for a board that will require a 10 year lifecycle. I'm wondering if you can provide lifecycle forecast information.
Thanks.
Part Number: ADS5263 Dear Sir or Madam,
why is there no bit for DITH_CH4 listed on the register addrees CB? pp.60 and pp.45.
Is enabling of dithering for individual channels possible?
Is CH4 "special" in this prospective?
Best
Part Number: ADS5263 Tool/software: Dear Sir or Madam,
I would like to operate the ADC in external voltage reference mode.
I have connected pin 56 to GND however I still see the VCM pin being a source of 1.5V. Is this expected? I would expect the…
Part Number: ADS5263 Tool/software: Dear Sir or Madam,
would it be possible to share some more insight into the internal CLK distribution structure to the 4 ADCs?
Is this a standard fan out? Are there other types of grouping - for example ADC1…
Part Number: ADS5263 Is there a Verilog HDL model for this ADC
ADS5263
? There is a thread on TI E2E forum but no one posted the model. Thanks on this support and request.
Part Number: ADS5263 Dear All,
I have used the eval board ADS5263-EVM at 110MSPS (datasheet states 100MSPS max) and the acq looks at the first glance OK. The power consumption goes up by app. 0.15W but I have not noticed any additional obvious problems…
Part Number: ADS5263
Hi Abhishek,
As you told it was capture issue we could solve it, thank you for your pointers.
Now, we're facing some more hiccups we're able to see sine wave in ila till 30 MHz sampling clock frequency from 40 MHz output is…
Part Number: ADS5263 Other Parts Discussed in Thread: ADS5294 hai,
There's no mention in ads5263 data sheet regarding how to configure it as bitwise mode and in one of the posts as i read writing the 0x28 register with 0x8100 will make it bit wise does…
Part Number: ADS5263 Other Parts Discussed in Thread: ADS5295 , Howdy,
As per the ADS5263 datasheet, specifically Register Address 12 shown on page 49, the Data, ADCLK, and LCLK LVDS outputs have programmable terminations. Is there an LVDS output buffer…