Hi KW,.
Thanks for the reply. Both of my USER_LED4 (D6) and USER_LED5 (D7) are off after I download the firmware to TSW1400. Also, I provide +5V to J1 and GND to J2 of the ADS5282, not 1.8V or 3.3V.
In the setup, I already turned the power of…
Hi,
The user guide for this EVM was probably written back when the TSW1200 was the commonly available capture card, but now we support that EVM with the TSW1400. one difference that I suspect might be hindering you is that the TSW1200 had FPGA firmware…
Other Parts Discussed in Thread: ADS5282 Hi,
I am intending to interface ADS5282 EVM with Altyera DE2-115 development board. Referring to the DE2_115_User_manual_2013, page # 41; Additionally, when LVDS is used as the I/O standard of the HSMC connector…
Hello,
I have a problem with the max. Voltage Peak to Peak with my ADS5282 EVM.
My System is a TSW1400 and a ADS5282 EVM.
As mentioned above is the max. Voltage peak to peak 2V with the internal reference.
But if I plug a Signalgenerator with…
Other Parts Discussed in Thread: ADS5282EVM , ADS5282
My customer is working on an investigation that requires simultaneous digitisation of at least 6 signals at a rate of at least 50 MSPS. Since it is a preliminary investigation, I prefer to use an…
Hi,
The AFE5805 is supported by the Medical Group, and as such any firmware for the TSW1405 for the AFE5805 would have to come from that group. So I am moving this posting to that forum. I do note that the sample data format for the AFE5805 is very…
Hi,
Understood. Thanks for your explanation.
Can you provide me TSW1400 source code ? It does work with ADS5282 EVM so part of it might be helpful for further development, right ?
Thanks.
Thanks for your reply Richard. I see in the datasheet of ADS5282 that the Analog Input Full-Scale Range: 2V PP and then in maximum ratings table it says -0.3V to 3.6V, can I use DC to 3.3V (0-3.3V) signal as input?
Hi,
So if you write x8110 you get a clock that is 12 * sampleclock? That would agree with the LVDS Timing Diagram on page 10, since this 10 bit device appends two zeros to the 10 bit data to output 12 bits.
The ADS5287 is a 10 bit version of the ADS5281…