Other Parts Discussed in Thread: ADS5292 Dear Tier.
I have one question for ADS5292.
Averaging mode is described as averaging two or four channels to improve SNR in the datasheet.
Btw, can I use this mode in the octal channel input system? I understand…
Other Parts Discussed in Thread: TX517 , AFE5809 , ADS52J90 , AFE5801EVM , AFE5801 , AFE58JD16 , AFE5816 , AFE5851 , ADS5294 , TX810
How to create an ultrasound system from TI’s ultrasound portfolio?
The signal chain would be TX517 -> transducer…
Is there a possibility i can have another TSW1250 ? I have the TSW1405 and a ADS5263, but it is not possible to connect to the ADC with that card.
Thanks,
Other Parts Discussed in Thread: ADS5292 , ADS5277 Hi..
I need your help!
What is the correct register value to test some function such as EN_RAMP, Dual_custom_PAT and Single_custom_pat in ADS5292?
In the datasheet, there are two registers. - 0x24…
Hi Niels,
Your observations are absolutely correct-there are discrepancies in this datasheet which we will try to eliminate in the next release. For clarification,
"960 MSPS" should read "960 Mbps" as you have indicated
It was determined during…
Hello,
I've a problem with this device. The sample rate is 42 MHz but the output bit clock is very slow, about 108 KHz:
-the imput clock is LVDS AC coupled 340 mV pk-pk;
-the power up process is correct, like the datasheet;
-the PD pin is shorted…
Other Parts Discussed in Thread: ADS5292 Do TI provide the LABVIEW drivers for communicating with this along with the evaluation board ??
I am doing a multi channel data acquisition system and will be using LV to control all the hardware. So it…
Part Number: ADS5294 Other Parts Discussed in Thread: ADS5292 Hi, the datasheet of the ADS5294 is describing a key feature "Oversampling to Minimize Harmonic Interference" and in figure 55 is a 12-tap filter shown. I have not found any documentation on…
Part Number: ADS5294 Other Parts Discussed in Thread: ADS5295 , ADS5292 , Hi.
In datasheet of ADS5295, it says that only 1-wire operation is possible in 16bit serialization mode.
But there is no such explanation in ads5292 or ads 5294 datasheet. …