Part Number: ADS5296A Other Parts Discussed in Thread: OPA4353 Datasheet has this note: "The external amplifier must provide an average current of 5 mA or less at the maximum sample rate."
Not sure how to interpret that. Do I need a wide-band…
Part Number: ADS5296A
I have the SDOUT driving a TXBN0304 to interface the 1.8V ADC's SPI to a 2.5V SPI bus and the voltage droops when not in readback mode.
The ADC establishes solid high and low levels during the read and while writing the register…
Part Number: ADS5296A Other Parts Discussed in Thread: THS4541 , Hi,
I have design with ADS5296A drive by 8 units of THS4541.
The feedback resistor of the THS4541 is 402 ohm per DS recommendation. (around 2.5 ma per amplifier for VCM drive)
The VCM drive…
Part Number: ADS5296A
I am looking at the setup and hold times for the case of 10x serialization in data sheet dated October 2013 (SBAS631).
On the one hand, the table on page 7 shows Tsu = 0.2 and Th = 0.16. These are defined in the figure 3.
Does this…
Part Number: ADS5296A Hi,
The table of pin descriptions on page 14 describes RESET (BAR) as active high reset yet the name indicates active low (BAR).
Figures 4 & 5 continue this confusion.
Could someone please tell me the correct polarity.
Than…
Part Number: ADS5296A Hello Team,
Good day.
My Customer who is working with a company designing a test socket for test QFN-64 pitch 0.5 would like to confirm some tolerance of the IC. It appears to them that the tolerance that appears in the datasheet…
Part Number: ADS5296A Other Parts Discussed in Thread: VCA2615 Hello TI.
Two questions:
Firstly :
I noticed that the EVM for this device uses back-back transformers at the input stage.
This idea is not mentioned in the data sheet.
Please tell me why the…
Part Number: ADS5296A I come from a telecommunications background where we developed bit error rate testers using pseudorandom bit sequences. The diversity of the bit sequences are superb for finding problems with too many consecutive ones or zeros as…
Part Number: ADS5296A In interleaved mode, two adjacent LVDS output streams deliver simultaneously the values of two successive samples. According to Figure 82 of the data sheet "Interleaving Mode Latency Timing Diagram", the lower-numbered output stream…
Part Number: ADS5296A The data sheet for the ADS5296A doesn't elaborate on the PRBS sequences and I cannot find a common reference for these patterns with a quick TI search. I'd love more detail.
Pseudorandom Bit Sequences are not standardized…