Part Number: TSW1400EVM Hi,
The aim is to evaluate the ADS5400.
1. Can the TSW1400EVM be directly connected to the ADS5400EVM and evaluate the ADS5400 ? If it can be evaluated,
2. Other If you have an environment that is necessary for evaluation, please…
Part Number: ADS5400EVM Other Parts Discussed in Thread: ADS5400 , LMK04806 , LMK04803 Hi,
I would like you to confirm evaluation environment for ADS5400 EVM.
1. According to user's guide of ADS5400 EVM, TI recommend to use TSW1200 to capture analog data…
Part Number: ADS5409 Other Parts Discussed in Thread: ADS5400 , , ADS54J60 We have the following requirements in a Measurement system where we are considering usage of either ADS5409 or ADS5400:
1) 4mV – 1Vpk-pk differential input amplitude support (It…
Part Number: ADS5400-SP The datasheet lists power supply current values for Fin=125MHz and Fs = 1GSPS as well as a sleep power dissipation value. What should I expect for typical and maximum power supply current values if I plan to operate the device at Fs…
Hi,
for an example of our FPGA firmware you could download the source code for the TSW1400 EVM on the TI web page for that FPGA Capture Card.
I do not see any reason why bit 5 should behave differently than all the other data output bits. Have you been…
Other Parts Discussed in Thread: ADS5400 , ADS5400EVM Hello,
I am working with the ADS5400 EVM and I am wondering whether is analog input can to be bipolar, unipolar, or both. In the slau293 document, it specifies to use a frequency generator set to a 0…
Hi,
the ADS5294 is not supported in the High Speed Data Converter forum, as that device is supported by the Medical group in their forum - even if the end application for the device might not really be medical. They are the ones who know the device. I…
Other Parts Discussed in Thread: ADS5400 , LMH5401 , TSW12J54EVM Now I am using ADS5400 to capture the input signal.
The characteristics of the input signal is as follow:
1) single-ended input, 50ohm;
2) signal bandwith :500MHz;
3) input voltage: -2V to…