Part Number: ADS5401 Tool/software: Team, My customer is asking us about ADS5401's temperature sensor. 1. What is the accuracy of the temperature sensor in ADS5401? 2. How can customer convert Reg 0x2B value to Celcius degree? - This may be answered in…
Part Number: ADS5401 Hi Sir,
We use the ADS5401 as an ADC input board, somehow, few of boards have observed a weird symptom, the lower 5 bit of output LVDS interface always "0".
We used the "Test Patten" function of the ADS5401 and got the same…
Part Number: ADS5401 Hello team,
I am using Keysight ADS to simulate IBIS model of ADS5401.
The termination resistor value cannot be selected, while the output current value is selectable.
Question:
Is our IBIS model for ADS5401 includes termination…
Part Number: ADS5402 The ground pins on the upper half of the part (like rows 10-14) seem like they really want to be analog ground since that is where the AVDD22, AVDD18, and INA_P/N powers and IF are. What would happen if those GND pins surrounding…
Part Number: ADS5401 Hi Sir,
recently, we found the VREF and VCM of ADS5401 equal to 0V when we power on it.
we'd like to know the section8.3, what will impact to voltage reference block? as my understanding, the reference voltage is a power circuit…
Hi Yusuf,
Please contact the product group about this model. They used Teraspeed to create a measurement based model.
We did not participate in the creation of this model.
David
Part Number: ADS5401 Dear Team,
The customer would like to use ADS5401.
The 12-Bit and 800-Msps is good for his design.
But I am wondering do we have price competitive device?
BR
Kevin
Hi,
in general, when there is a differential input that left open circuit or disconnected then what can happen is that the differential voltage across the pins could drift to about 0V across the pins, and then the input buffer can begin to 'chatter…
Hi Yusuf,
I am asking about the aperture delay from the sampling clock input to the actual sampling moment. I can not find it in the ADS5401 datasheet, so it is probably not characterized unlike for other TI ADCs. for example:
Here is the definition…