Part Number: TSW14DL3200EVM Other Parts Discussed in Thread: ADC12DL3200EVM , ADC12DL3200 , FMC-ADC-ADAPTER , ADS5402 , ADS5407 What TI A/D and D/A converter evaluation kits are compatible with this evaluation board? I am especially interested in DAC3482EVM…
Hi Richard,
Thanks very much for your time and troubleshooting instructions. I find that the SPI connection to LMK is active. The current drawn by the board at bias voltage of 6V drops to 0.92A from 1.3A while LMK is powered down through the GUI. I set…
Hi, thanks for the quick reply. Is the TSW1400EVM also able to capture data from two channels with 800 MSPS and 12 Bits each like for the ADS5402? Or is it able to capture only one channel with 800 MSPS? Best regards Benjamin
Other Parts Discussed in Thread: ADS5402 Hello.
In my board i use dual balun ETC1-1-13 identical matching circuit as EVM board for ADS5402 EVM.
Impedance matched to the load 50, but I see that input signal level decreases by 6 dB.
What could be the cause of…
3806.slwu087d.pdf Nikunj,
If you are using a coherent IF input, the exact frequency value needs to be entered for the ADC target input frequency. If you are not using a coherent input, you can leave this blank. See the HSDC Pro GUI User's Guide (attached…
Other Parts Discussed in Thread: ADS5402 Hi
I am working with TSW1266 receiver.
Kindly let me know how RF to IF conversion process taking place?
Can I change the IF frequency in TSW1266?
Thanks a lot
Girish
Other Parts Discussed in Thread: ADS5402 , LMK04808 hello,
I am using TSW1266 EVM with TSW1400 EVM FPGA and I was previously using the default settings of TSW1266 EVM from it's users manual which is working at 614.4MHz sampling rate and the settings…
Other Parts Discussed in Thread: ADS5474 , ADS5402 , ADC12D500RF Hi,
I'm seeking for dual channels,12bits and over,400MSPS and over ADC with small latency like ADS5474. Would you provide the information ?
Best Regards,
Kato
Other Parts Discussed in Thread: ADS5402 , ADS5400 , ADC08D500 I think the Subject line asks the question succinctly... I want to use multiple lower cost ~100Msps ADCs sequenced properly to achieve an overall sampling rate of 800Msps or greater. Another…