Part Number: ADS5409EVM Hello,
I am working on a project that requires the rapid acquisition of analog data, and I may consider using an ADC evaluation board along with the associated data capture card. My application aims to retrieve data from a sensor…
Part Number: ADS5409EVM Other Parts Discussed in Thread: LMX2572 Hello, I am using ADS5409EVM ADC Board and TSW1400EVM Capture Board. For the use of these boards, I need to generate a clock signal at 900MHz. However, it is said that the amplitude of this…
Part Number: ADS5409EVM Hello, is there a chance to set the default firmware for the TSW1400EVM Capture Card? Can I permanently load one of the RBF firmwares onto this kit using HSDC Pro or a different GUI? If I can't load it, which SPI pins are used…
Part Number: ADS5409EVM Other Parts Discussed in Thread: CDCE62005EVM , CDCM9102 , CDCE62005
Hello,
I have purchased the ADS5409EVM and TSW1400EVM kits. I have connected these kits to each other using the relevant interface points. After…
Part Number: ADS5409EVM Other Parts Discussed in Thread: ADS5402EVM , ADS5409 The ADS5409EVM (same as ADS5402EVM) appears to be driving the ADC’s SCLK, SDIO, and SDENB pins with 3.3V levels in violation of the ADC’s absolute maximum input voltage levels…
Part Number: ADS5409EVM Other Parts Discussed in Thread: HSMC-ADC-BRIDGE , ADS5409 Hello,
My customer has a question about ADS5409EVM.
[Q]
Can it connect to Altera development board with HSMC-ADC-BRIDGE ?
Best Regards,
Hiroshi Katsunaga
Other Parts Discussed in Thread: ADS5409EVM Could you tell us trace length of DATA and CLOCK between U1 and J11 of ADS5409EVM board?
CVS or TXT report file from the CAD tool will be grate.
Other Parts Discussed in Thread: ADS5409EVM Hello,
I have ADS5409EVM and TSW1400EVM. I want to capture data from TSW1400EVM by using Jetson Orin Nano (Linux). I can't find .so files for Linux in High-Speed Data Converter application. Where can I find…
Part Number: LMX2572EVM Other Parts Discussed in Thread: ADS5409EVM , Hello, I need to provide a 1GHz clock for my ADS5409EVM board and I decided to buy the LMX2572EVM board. But do I need to buy another external card for this card? Does the LMX2572EVM…
Robert,
Do you need 14 bits? Or can you get by with 12 bits? Maybe the below might be ok for your project. Check out the specs.
http://www.ti.com/tool/ads5409evm
Ken.