Part Number: ADS5463 Tool/software: Hi,
I'm thinking to design ADS5463 custom board but I'm confused for couple of questions.
What is the material of EVM board? Can you give full name of FR-4 Material?
Is this ADC suitable with XC7Z020-1CLG484C…
Part Number: ADS5463-SP Hello, The datasheet specifies ADS5463-SP power dissipation is 2.45W(max) at Vin=full scale, fin=300MHz and Fs=500MSPS. My customer plans to use ADS5463-SP at 100MSPS. How much would the power dissipation be? Best regards, K…
Part Number: ADS5463 Hello Ti's team I am Anh Nguyen, Viettel group, Viet Nam. We are intending to buy ADC partnumber: ADS5463. Can you recommend us a chip part number suitable for this type of ADC, the type of chip that can capture the output signal…
Part Number: ADS5463 Hi Sir,
Could you please help recommend the PCB layout requirement for the ADS5463?
What's the impedance for the input PCB trace for the ADS5463 pin16 and pin17 ?
Do I need to use microstrip?
Do I need add void under the input…
Part Number: ADS5463-SP Hi, Is there any data available relating to shock & vibration on ADS5463-SP?
Does the test documents for ADS5463-SP 5962R0720802VXC cover this info?
Part Number: ADS5463 Hi Team,
A customer ordered ADS5463EVM which is to be operated with 100 MHz FPGA card. The sampling rate of the ADS5463 is 500 MSPS. They want to know whether or not the 100MHz FPGA card misses any data sampled with 500MSPS by ADS5463…
Part Number: ADS5463-SP Hello team,
My customer has a question about single-ended input of ADS5463-SP.
This ADC is a differential input type, but is it possible to use it for a single-ended input signal?
In the data sheet application, a transformer or…
Part Number: ADS5463 Hi Team,
This is customer request, can you please advise:
"
1-) We are getting ADS5463EVM from Texas. This 500 MSPS contains an adc. But we will work with 100 MHz. So adc will work faster than us. But in the adc's datasheet,…
Part Number: ADS5463-EP Other Parts Discussed in Thread: ADS5463 Hello,
We have some old ADC Modules, designed and built with ADS54RF63IPFP, that worked well over the years.
Now we plan to make more of the same, and we're thinking to use ADS5463MPFPEP…
Part Number: ADS5463-SP Could you let me know the package information as follows?
P/N: 5962R0720802VXC
・Package material/ base plating /plating (ex. Ceramic(Alumina)/Ni/Au
・Lid material/ base plating /plating (ex. Covar/Ni/Au
・Package cavity wall thickness…