Part Number: ADS5463
Hello,
I am planning to interface ADS546 3 and DAC3152 using an FPGA board between the data converters. I need an FPGA board to perform some operations on the data from ADC and pass the new data to DAC. I am going to interface the boards…
Part Number: ADS5463-EP Hi there:
In the datasheet of ADS5463-EP, there is only a typical value of clock input amplitude, which is 3V Vpp (differential sine wave, in datasheet Page 5).
This value doesn't show the minimum limit, where will effect the…
Part Number: ADS5463 Other Parts Discussed in Thread: TIDA-00069
Hi,
we want to connect ADS5463 (12bit,500Msps and parallel LVDS Output) to Xilinx SOC chip, but I don't have idea about parallel LVDS.
1) I find and read some thing about serial LVDS…
Other Parts Discussed in Thread: ADS5463 , ADS4149EVM , ADS4149 , ADC12D500RF , ADC12D800RF , ADC12J4000EVM , ADC12J4000 Thanks for the answer.
I just want to ask you one more question. The ADC of the ADS5463 has a bandwidth of up to 2.3 GHz, It has a clock input…
Other Parts Discussed in Thread: ADS5463 Now, I am using ADS5463, and the data out of it is input to XC7V690T.
The same program sometimes get OK data, but, sometimes is NOT OK,
Figure 1 Data is not OK.
Figure 2 Data is OK.
Why?
Thanks for your help…
Part Number: HSMC-ADC-BRIDGE Other Parts Discussed in Thread: ADS5463 Hi,
I am trying to aquire data from the above configuration using a Altera Arrow SoCKit. The schematic from both boards shows that they are compatible.(I think)
https://rocketboards…
Other Parts Discussed in Thread: ADS5463 , ADS5474 Hello,
My customer has some questions about ADS5463 thermal parameters.
[Q] Do you have the following parameters ?
・RθJC(top)
・ΨJT
・ΨJB
Best Regards,
Hiroshi Katsunaga
Other Parts Discussed in Thread: ADS5463-SP Hi,
My custmer is using ADS5463-SP. They have the below questions about package. Could you answer me this questions, please?
Q1:Is Heat slug Floting Metal?
Q2:Could you let me know material of heat slug? -> Conductor…