Hello,
I am trying to use the same ADC ADS5463 with altera de-2 115 dev board. Would you be able to provide an example for this platform?
Many thanks,
Michal
Part Number: ADS41B29 Other Parts Discussed in Thread: ADS4129 , ADS5463 Dear Expert
There is a curve in the specification that I didn't understand: the relationship between input voltage and SNR. Why does the larger the input amplitude, the lower the SNR…
Other Parts Discussed in Thread: ADS5463-SP Hi,
I required information related to ADS5463-SP. Please confirm whether it has a thermal pad. If so, what is the dimension of the thermal pad?
Also, please provide information as to where it has to be connected…
Other Parts Discussed in Thread: ADS5463 I recently attached a ADS5463 EVM board to a Altera Cyclone V GX board via HSMC-ADC bridge. This Cyclone GX acquires data on the positive edge of each clock cycle (125 MHz) for about 30 samples. Then sends the data…
Other Parts Discussed in Thread: ADS5463-SP Hi, I would like to know which is the output format of the ADS5463-SP.
In the datasheet "Offset Binary" is specified, but I can't find if it's "Bipolar Offset Binary" or "Complementary Offest Binary" as defined…
Other Parts Discussed in Thread: ADS5463-SP Hello Team,
My customer ALTER has a question regarding the ADS5463-SP they are already using and they want to use in a flight application. They are using ADS5463-SP for an application that does not convert continuously…
Hi Richard,
Thanks for replying again. Yes, you had posted this sketch on a different post too. I am trying to use this implementation for my interfacing. At the same time, I would also like to get the VHDL source code used in the TSW1200 capture cards…
Wade,
My question concerns ADS54xx (ie ADS5463)
Could you confirm that the clock inputs (differential ac) are not compatible ( LVDS ) ?
In this case, that are the solutions to drive theses inputs.(without RF transform or Balun solution)
I have the same…
Other Parts Discussed in Thread: ADS5463-SP Hi,
Are the two RESERVED pins (31 & 35) totally unconnected within the ADS5463-SP package, or are they attached to some internal voltage potential, test point, or other logic?