Other Parts Discussed in Thread: ADS5463-SP Hi,
Are the two RESERVED pins (31 & 35) totally unconnected within the ADS5463-SP package, or are they attached to some internal voltage potential, test point, or other logic?
Other Parts Discussed in Thread: ADS5463 , ADS5463EVM , ADS54RF63EVM , ADS54RF63 Hello,
I am running into a nasty glitching problem with
ADS5463. After spending quite a bit of time looking for some problem in
my hardware or logic I am convinced the…
Other Parts Discussed in Thread: ADS5463 Hi,
I have some question regarding the testing of the ADS5463:
Sampling rate is ~410Mbps.
Noise floor ~ -70dB.
The SNR achieved > 65dB
Single tone SFDR
In -1dBFS input power the SFDR is 55…
Other Parts Discussed in Thread: ADS5463 Can i use ADS5463 with a variable clock? i mean, a clock whose frequency changes from, e.g, 100Mhz to 350Mhz?
well, the change is not jumpy, but rather smoothly up and down
is there gonna be adverse effect…
Other Parts Discussed in Thread: ADS5463-SP Hi,
Does any know where I can get information about ADS5463-SP SEE (Singe Event Effects) ?
I read this datasheet and its only specifies that TID is 100 Krads.
Thank you
Jonathan,
For ADS54RF63 min speed is 40Mhz and 20Mhz is for ADS5463. We had tested these speed and you should have performance in spec at 20 Mhz of ADS5463, but you could see the performance lower than it at 450MSPS. This is shown in the figure 25…
Other Parts Discussed in Thread: ADS5463 , ADS5463EVM I need to convert a wide-bandwidth signal, using a rapidly varying sample clock. The ADS5463 accepts a sample clock from 20MHz to 500MHz using a pipelined converter, with 3.5 cycles of latency, producing…
Other Parts Discussed in Thread: ADS5463-SP On page 18 of the ADS5463-SP datasheet it states that the DRY signal should be used to capture the DATA out of the ADC. However, when I look on page 9 of the datasheet and review the timing information it appears…
Other Parts Discussed in Thread: ADS5463 , PGA870 Hello!
Problems with ADC ADS5463 Friends, help to understand the problem. Translate simple input, to output A/D CONVERTERS for 250 units of data removed.
Shifting constantly. CLKIN = 65 MHz, Vref…
Other Parts Discussed in Thread: THS4513 , THS4513-SP , THS4509 , ADS5463-SP , TINA-TI Hello,
TI had suggested using the THS4513 (or THS4511 ) amp to drive an ADC. Our ADC selection is the TI ADS5463-SP . On page 17 of the ADS5463-SP data sheet an example…