Part Number: ADS5474 Hello, I was wondering if the about heat sink and lid grounding? Are either grounded? Or does the sink need to be grounded to achieve grounding for both?
Part Number: ADS5474 Hi,
In the datasheed for ADS5474 the figure 45 shows SNR vs Input Frequency and External Clock Jitter with measurements up to 200-fs jitter.
How can user estimate SNR degradation if the jitter is up to 850-fs?
Thanks.
Part Number: ADS5474-SP Im looking at these flight parts:
P/N: 5962R1320801VXC
P/N: ADS5474MHFGV
The technical details seems to be identical however is there any difference between the screening flow?
My pkg lead told me that ADS5474MHFGV does not have…
Part Number: ADS5474-SP Hello,
Is it correct that all three orderable P/N devices below for the ADS5474-SP have the same pin allocation in the same package?
My customer wants to mix and match in one design according to the required specifications.
Thanks…
Part Number: ADS5474 Hi Exeprts,
We have a question about ADS5474 from customer:
Scheme consist of signal generator -> ADS5474 -> FPGA kintex7 xc7k325t.
I drive AIN_p and AIN_n signal with power -26 dbm, freq 100 khz, plot fft from ila data and…
Part Number: ADS5474 Other Parts Discussed in Thread: LMK1D1208I , CDCLVD2106 , LMK00725 Hi Experts,
I need help choosing a clock for the part ADS5474IPFP from 120mhz. It has that 3.1V offset and I'm not familiar with the options for this. I think it may…
Part Number: ADS5474 Hi everyone,
We are considering to include the part ADS5474IPFP in several designs, which will have a long life. The part fits with our design needs and, based in previuos experiencies, we feel comfortable with its performance. Nevertheless…
Part Number: ADS5474 Hi Experts, Good day. The customer is asking about the figure 43 in the data sheet shows VCM as 2.5V but everywhere else in the document its 3.1V? Is it possible to set it to 2.5V? Please advise. Please advise. Regards, Josel
Part Number: ADS5474 Hi,
We want to measure pulse width with adc. The incoming pulse signal is maximum 200MHz(>5ns pulse).The ADS5474 seems suitable for this job.
But we have 2 important criteria; 1) We want to do this work with Mcu. Mcu connection…