Part Number: ADS5481 What is the frequency range of the internal dither feature? Our lowest ADC input frequency is 1MHz, so we're hoping the dither frequencies are well below that. Thanks.
Other Parts Discussed in Thread: ADS5481 Hi ,
I am looking for the ADS5481 QFN64 footprint symbol. Unable to locate it on the website. I plan to interface it with an FPGA for DSP applications on FPGA.
Hi Kang,
Another TI ADC describes the AC and DC components on two different max absolutes ratings.
www.ti.com/.../ads5481.pdf
Is that the same thing with the ADS41B49?
Should it be AC signal component only max rating to 1.9V and not take into…
Hi Matteo,
Oh yes, good catch - you are correct. I used the NSD value for the ADC3561 (-150 dBFS/Hz). Yes please substitute the -158 dBFS/Hz for the ADC3563 into the equation.
I did a search with these parameters on our device page. I had to back…
Hi Thinh,
Please let me know if increasing the clock amplitude has any effect on your data capture.
1. We have not had any reported issues using HSDC Pro with Windows 10.
2. The datasheet is not explicit with this information, and can only guarantee…
Other Parts Discussed in Thread: ADS5481 , ADS5560 Hi Team,
My customer considers to use AD7626 for his system. http://www.analog.com/media/en/technical-documentation/data-sheets/AD7626.pdf
Could you please let me know whether TI has any alternative…
Hi,
If none of that bank of LEDs are lit then I would suspect the FPGA does not have its bit file loaded, but in that case the GUI should not let you click the capture button. Perhaps i could see a screenshot of the HSDCPro - i would be looking for…
Other Parts Discussed in Thread: ADS5482 , ADS5484 , ADS5485 , ADS5481 , ADS5483 I am working on PCB design that uses high speed 16-bit ADC family from TI, Part number ADS5481, ADS5482, ADS5483, ADS5484, ADS5485 ….
1) Question 1: Is recommended to…
Are there any instructions for using the ADS548xEVM with the TSW1400 host board?
The instructions that I could find were all for the obsolete 1200 board.
I managed to get things working, but I'm not sure if I did it right.
Hardware mod: Bend J13…