Part Number: ADS54J40 Other Parts Discussed in Thread: ADS54J60 Hello,
In the attached file under the Freeze IL Engine on page 2 the following lines are listed:
0: 0x4005 0x01 // Enable single channel writes 1: 0x4004 0x61 2: 0x4003 0x00 3: 0x4002 0x05 4:…
Part Number: ADS54J40 DEARS.
I am reviewing ADS54J40 design.
My setup is as follows.
MSPS Range : 100MSPS to 600MSPS INPUT IF : 368.64Mhz INPUT TYPE : REAL Band Width : 100Mhz Sampling Clock : 491.52Mhz Decimation : 2 ADC NCO : -122.88Mhz LMFS : 4222
I am confused…
Part Number: ADS54J40 The datasheet, chapter 9.2 "Typical Application" shows a diagram without 100ohm termination of the input clock. However the EVM "ADS54J40EVM " has a termination on the PCB. So I'm confused, I cannot find it in the datasheet.…
Part Number: ADS54J40 Other Parts Discussed in Thread: ADC32RF45 , Hi
I see that the ENOB for the ADS54J40 is 11.2 whereas for the ADC32RF45 is 9.7. I wanted to check if the low ENOB for the ADC32RF45 is only this low at the max rate of 3GSPS i.e. if I…
Part Number: ADS54J40 Hi all,
Our customer designing the analytical instrument is looking for an ADC with the functionality shown in the title.
/ CNVST PIN (Low aperture delay) / shorter acquisition time specs / pipeline latency is no problem These features…
Part Number: ADS54J20 Other Parts Discussed in Thread: ADS54J60 Hello,
It seems that these devices are quite similar.
1) Can you please confirm they're pin compatible? Drop in compatible?
If not ,what are the differences?
2) I intend to implement…
Part Number: ADS54J40 Dears,
Avnet EUC team request TI confirmation evidence for ADS54J40IRMP
Now customer had review severl TI solution for their new test equipment solution which is EMC measurement.
Pls reply to me as below request.
ECCN 3A001.a.5 …
Part Number: ADS54J60EVM Other Parts Discussed in Thread: LMK04828 Hi everyone,
We are facing a strange issue with our ADS54J60EVM FMC ADC. While sampling our input signal that varies from 20mVpp up to 1.9Vpp (the maximum swing that should in theory give…
Part Number: ADS54J40 Other Parts Discussed in Thread: ADC12D1000 , ADC12D800RF Hi
I am planning to spin my custom board with an FMC connector with the ADS54J40 and was wondering if I would need to purchase the JESD204 IP Core Licence from Xilinx if I…
Part Number: ADS54J40 Dear e2e Support,
My customer need a HS-ADC with the following requirements:
Fs 800MHz
12 or 14 bits
need to work on the 3rd Nyquist Band (800 to 1000Mhz at least)
We've selected the ADS54J40. Is that coherent?
The fact is…