Part Number: TSW14J56EVM Hi,
To evaluate the performance of ADC Module ADS54J66, i have procured ADS54J66 + TSW14J56 Combo
I have biased both of the boards with 5V/4A(CurrentLimit) Supplies
Connected both of the boards USB to my PC
Ran the HSDC Pro V5…
Part Number: ADS54J66
Hi
I am using ADS54J66 ADC in my application.
1 . I am operating ADC in Mode 2 (Decimation = 2).
Clock to the ADC = 400 MHz.
Now what is my Sampling Rate for each channel ??
Is it 200 MHz or 400 MHz ? (Single we are decimating…
Part Number: ADS54J66 Hi Sir,
For registers LC[23:0] and HC[23:0], do they mean the LMFC count? How can I configure them correctly?
Is there any guidelines for our information?
Sincerely,
LB Shi
Part Number: ADS54J66 Hi
Let me Know the termination required for SYNbAB & SYNbCD pins.
Datasheet recommends to provide termination and also in Figure 144. Application Diagram for the ADS54J66, it is mentioned to provide 1.2V.
Kindly provide the value…
Part Number: ADS54J66 Hi Sir,
In our project, we want to achieve power-up deterministic phase by JESD204B. However, till now, the power-up phase is not deterministic.
We'd like to check the status of SYSREF± to know if the SYSREF± signal is captured…
Part Number: ADS54J66
Hi
I am using ADS54J66 in my application.
Common Mode voltage = 2v
peak to Peak = 1.9v
So at the ADC input, if we probe we will get voltage from 2 - (pk_to_pk / 2) to 2 + (pk_to_pk / 2) ie.. from 1.05 to 2.95 . Right ??
Also …
Part Number: ADS54J66 Hi
In the ADS54J66 datasheet, I found these Specifications
All the Spectifications are in dBFS
I am confused of this conversion.
Can you guide me with the conversion from dBFS to dB ?
Part Number: ADS54J66 Other Parts Discussed in Thread: ADS54J64 Hi
In my Application, I want to sample CCD waveform.
Image of CCD waveform is shown below.
Can I use ADS54J66 to Sample this kind of waveform??
Will there be any complications ?
Part Number: ADS54J66 Hi,
For ADS54J66 Quad Channel ADC front end design, s-Parameter files required for Differential analog input channels A, B, C & D.
With Regards,
Vigneshwar Raj D