Part Number: ADS54J69 Other Parts Discussed in Thread: LMK04828 , , Dear TI experts,
My customer now tests ADS54J69 with LMK04828 and xilinx FPGA (use JESD204B)
the block diagram is as below;
They confirmed FPGA_JESD_CLK as 100MHz. (it is okay…
Part Number: ADS54J69 Other Parts Discussed in Thread: ADS54J60 Hello,
We have an application where we'd like to operate the ADS54J69 at a rate below 250MSPS, but the datasheet seems to imply that the device is not capable of using an input clock of…
Part Number: ADS54J69 Other Parts Discussed in Thread: ADS54J60
Hi Team,
Use ads54j69 to achieve baseband bandwidth of more than 320M sampling.
Can the Jesd204b link only be configured for 4222 and 2242 modes? Thanks.
Among the four outputs, can…
Part Number: ADS54J69 Other Parts Discussed in Thread: ADS54J60 , Hi Team,
How to shut up DECIMATION?
Can the configuration be turned off as others? Thanks.
Best Regards
Charlie Xiao
Part Number: ADS54J69 Hello,
One customer used ADS54J69 and met questions as following:
1. Configure the ADC with 4222 mode, Reg 0x52=0x08,0x72=0x08. According to Figre74, it should output from Lane0 and Lane1. But actually, lane 1, lane2 and lane…
Part Number: ADS54J69 Hi team,
Does ADS54J69 input clock (device clock and SYSREF clock) accept either LVDS or LVPECL?
It looks like the datasheet p.7 mentions it accepts both of them.
But it is not clearly stated so I'd like to make it sure.…
Part Number: ADS54J69 I am designing an ADC based board in which I have used ads54j69 ADC.
Most of the circuitry I copied from the evaluation board.
since I am designing the board to qualify for mil grade, for which temperature requirement is min…
Part Number: ADS54J69 Other Parts Discussed in Thread: ADS54J60 , Hi Team,
We have received this inquiry from our customer,
In the ADS54J60 datasheet, page 72 mentions the register 068h that allows to freeze the DC Offset correction.
1- Is this…
Part Number: ADS54J69 Other Parts Discussed in Thread: LMK04610 Dear sir:
I am panxiaohong in the china。
I used the ADS54J69 in the project to convert analog singal to digital。
Now I met a question as below,
The CLKINP(PIN 27) and CLKINM(PIN 28…
Part Number: ADS54J69 HI:
I am using the ADC ADS54J69 to design our ADC product. And the anlog input end's picture is as bleow:
I met some question:
When we input sine wave signal( it is 10Mhz,1.23Vp-p), after we insert the J701 connector, the input…