Part Number: ADS54RF63 Hi,
We are using the ADS54RF63 in combination with a Xilinx xc7k160tffg676-2 FPGA. The routes on the board are 100 Ohm differential and the termination resistor in the FPGA are on. Nevertheless we see reflections on the ADC outputs…
Part Number: ADS5282
I am working on a project that involves SP605 xilinx eval board and an ADS54RF63EVM ADC eval module (along with the ADC to FMC passive adapter board). I'd like to capture ADC output and send it out of the gigabit ethernet interface…
Hi,
I am using Virtex 6 ML605 board to latch the digital output data coming from ADS54RF63EVM. It would be really helpful if I could get in touch with fellow users with respect to this issue. I am facing quite a lot of fundamental issues with respect…
I've recently bought a SP605 xilinx eval board and an ADS54RF63EVM ADC eval module (along with the ADC to FMC passive adapter board). I'd like to capture ADC output and send it out of the gigabit ethernet interface on the sp605. Would the code you are…
Hi Richard,
I went on to interface the ADS54RF63EVM board and DAC34SH84EVM board with a Xilinx Virtex 6 ML605 board. 1. I am using the 19.2 MHz crystal source inside the DAC34SH84 to generate a 270 MHz clock for both the DAC board, and FPGA board…
Other Parts Discussed in Thread: ADS54RF63EVM Hi,
System involved : ADS54RF63EVM (12 bit parallel LVDS output) -> V6 Ml605 -> DAC34SH84EVM (16 bit parallel )
Problem : I am giving a 17 Mhz ( 2 Vp-p) sinewave to the input of the ADC, and I expect…
Other Parts Discussed in Thread: ADS54RF63EVM Hi,
Whilst reading this post http://e2e.ti.com/support/data_converters/high_speed_data_converters/f/68/t/47555.aspx?PageIndex=2 I saw that you have some example VHDL for a different ADC. I am trying…
A few more bits of data:
1. ADS54RF63EVM also has glitches, but at a lower rate and amplitude at 500 MHz.
2. On ADS54RF63EVM at 544 MHz the error rate is sensitive to the device temperature (9e-7 glitch rate drops to 6e-7 going from 45degC to 28degC…